Part Number: AM625
Dear TI Expert,
SW : Processor SDK 8.5
HW : AM62-SKEVM rev E3
Boot mode : eMMC
I'm checking the booting time on EVM and using eMMC for boot.
However, it takes a lot of time(1.3sec) between A53 SPL and A53 U-Boot as shown in the log below.()
[0.863986 0.000098] U-Boot SPL 2021.01-00001-g3e29ce144c (Feb 16 2023 - 15:35:12 +0900)
[0.866361 0.002375] SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
[0.927521 0.061160] Trying to boot from MMC1
[2.207378 1.279857]
[2.207499 0.000121]
[2.207553 0.000054] U-Boot 2021.01-00001-g3e29ce144c (Feb 16 2023 - 15:35:12 +0900)
jwook@jwook-Desktop:~$ grabserial -d /dev/ttyUSB0 -t [0.000001 0.000001] [0.159659 0.159658] U-Boot SPL 2021.01-00001-g3e29ce144c (Feb 16 2023 - 16:45:02 +0900) [0.174948 0.015289] SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar') [0.222873 0.047926] SPL initial stack usage: 13424 bytes [0.238958 0.016085] Trying to boot from MMC1 [0.367542 0.128584] Loading Environment from MMC... OK [0.479892 0.112349] init_env from device 9 not supported! [0.495928 0.016037] Starting ATF on ARM64 core... [0.497019 0.001091] [0.497065 0.000046] NOTICE: BL31: v2.7(release):v2.7.0-359-g1309c6c805-dirty [0.511551 0.014486] NOTICE: BL31: Built : 11:48:12, Dec 14 2022 [0.526910 0.015359] I/TC: [0.527226 0.000316] I/TC: OP-TEE version: 3.19.0-15-gd6c5d0037 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Wed Dec 14 11:52:03 UTC 2022 aarch64 [0.547191 0.019965] I/TC: WARNING: This OP-TEE configuration might be insecure! [0.559039 0.011848] I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html [0.559802 0.000763] I/TC: Primary CPU initializing [0.560003 0.000201] I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar') [0.575335 0.015332] I/TC: HUK Initialized [0.575485 0.000150] I/TC: Activated SA2UL device [0.575672 0.000186] I/TC: Fixing SA2UL firewall owner for GP device [0.575978 0.000306] I/TC: Enabled firewalls for SA2UL TRNG device [0.591151 0.015174] I/TC: SA2UL TRNG initialized [0.591386 0.000235] I/TC: SA2UL Drivers initialized [0.591688 0.000303] I/TC: Primary CPU switching to normal world boot [0.863888 0.272199] [0.863986 0.000098] U-Boot SPL 2021.01-00001-g3e29ce144c (Feb 16 2023 - 15:35:12 +0900) [0.866361 0.002375] SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar') [0.927521 0.061160] Trying to boot from MMC1 [2.207378 1.279857] [2.207499 0.000121] [2.207553 0.000054] U-Boot 2021.01-00001-g3e29ce144c (Feb 16 2023 - 15:35:12 +0900) [2.224181 0.016628] [2.224194 0.000013] SoC: AM62X SR1.0 GP [2.224350 0.000156] Model: Texas Instruments AM625 SK [2.271379 0.047028] EEPROM not available at 0x50, trying to read at 0x51 [2.302705 0.031327] Board: AM62-SKEVM rev E3 [2.303161 0.000456] DRAM: 2 GiB [2.510875 0.207714] MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2 [2.512778 0.001902] Loading Environment from MMC... OK [2.607454 0.094676] In: serial@2800000 [2.608266 0.000812] Out: serial@2800000 [2.609070 0.000804] Err: serial@2800000 [2.622718 0.013647] Net: eth0: ethernet@8000000port@1 [2.624182 0.001465] Hit any key to stop autoboot: 0
Is this expected result?
Please let me know how to reduce the boot time between them if you have.
Thanks&Regards,
Jaewook