Hi all,
I have an OMAP3530 EVM Rev G Board from Mistral and I am using OMAP Linux PSP version 02.01.03.11. For our project purpose, we need to enable OMAP3530 to work as USB device and support isochronous transfer from device to host. As per OMAP Linux PSP datasheet, the musb driver supports isochronous devices under host mode only.
Is there any patch available for enabling isochronous transfer support for OMAP3530 under device mode? I am now blocked in this issue. Please help me solve this issue. Our project schedule is so tight. :(
Thanks in advance,
Honey S