Hi,
We are using a custom board based on am5708 and using ti-processor-sdk-linux-am57xx-hs-evm-08_02_01_00.
We have generated MLO, u-boot.img, kernel and rootfs using SDK.
We flash the wic image generated by SDK onto the sd card and the board is booting perfectly fine. The following is the partition scheme:
Disk /dev/mmcblk1: 30 GB, 31914983424 bytes, 62333952 sectors 486984 cylinders, 4 heads, 32 sectors/track Units: sectors of 1 * 512 = 512 bytes Device Boot StartCHS EndCHS StartLBA EndLBA Sectors Size Id Type /dev/mmcblk1p1 * 384,0,1 639,3,32 49152 81919 32768 16.0M c Win95 FAT32 (LBA) /dev/mmcblk1p2 640,0,1 1023,3,32 81920 4095999 4014080 1960M 83 Linux /dev/mmcblk1p3 1023,3,32 1023,3,32 4096000 8110079 4014080 1960M 83 Linux /dev/mmcblk1p4 1023,3,32 1023,3,32 8110080 8372223 262144 128M 83 Linux
We copy the same wic image on the SD card and flash (using "dd" command) it onto the emmc. It also has the similar partition scheme.
Disk /dev/mmcblk0: 7456 MB, 7818182656 bytes, 15269888 sectors 119296 cylinders, 4 heads, 32 sectors/track Units: sectors of 1 * 512 = 512 bytes Device Boot StartCHS EndCHS StartLBA EndLBA Sectors Size Id Type /dev/mmcblk0p1 * 384,0,1 639,3,32 49152 81919 32768 16.0M c Win95 FAT32 (LBA) /dev/mmcblk0p2 640,0,1 1023,3,32 81920 4095999 4014080 1960M 83 Linux /dev/mmcblk0p3 1023,3,32 1023,3,32 4096000 8110079 4014080 1960M 83 Linux /dev/mmcblk0p4 1023,3,32 1023,3,32 8110080 8372223 262144 128M 83 Linux
But u-boot wont come up with eMMC. It stops at SPL and here is the log:
PPA 4.6.4 (GCC Build - Sep 24 2020 - 16:41:23) Supports ALL DRA7x, TDA2x, and AM57x devices Detected device: 05841e21 HS !ONLY PUBLIC DEBUG ON! !OBFUSCATOR ON! !TEE Load API SUPPORTED! SEC_STATUS = 0x23820081 SEC_CTRL = 0x00010203 SEC_EMU = 0x000007fc SEC_TAP = 0x00002607 U-Boot SPL 2021.01-g91d7e1a7ab (Apr 10 2023 - 09:38:44 +0000) DRA722-HS ES2.1 Trying to boot from MMC2_2 ** Partition 1 not valid on device 1 ** spl_register_fat_device: fat register err - -1 spl_load_image_fat: error reading image u-boot.img, err - -1 spl: no partition table found SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
I tried to follow this link:
but ended up getting these security events:
PPA 4.6.4 (GCC Build - Sep 24 2020 - 16:41:23) Supports ALL DRA7x, TDA2x, and AM57x devices Detected device: 05841e21 HS !ONLY PUBLIC DEBUG ON! !OBFUSCATOR ON! !TEE Load API SUPPORTED! SEC_STATUS = 0x2282f8a2 SEC_CTRL = 0x00010203 SEC_EMU = 0x000007fc SEC_TAP = 0x00002607 U-Boot SPL 2021.01-g91d7e1a7ab (Apr 10 2023 - 09:38:44 +0000) DRA722-HS ES2.1 Trying to boot from MMC2_2 no pinctrl state for default mode -- NON SECURE CODE GENERATED A SECURITY VIOLATION -- -- WARNING: violation might be due to speculative accesses. Check L3 interconnect -- PPA cleans FW and CONTROL module registers & let the NS alive. CONTROL_SEC_ERR_STATUS_FUNC = 00000800 CONTROL_SEC_ERR_STATUS_FUNC_2 = 00000000 Interrupted context: r0=4037f064, r1=81fffe54, r2=4037bc24, r3=80800000, r4=81fffee4, r5=4031df6e, r6=00000000, r7=4031754f, r8=81fffee0, r9=81ffff20, r10=fffff44b, r11=00000000, r12=81f003d0, lr_fiq=40301370, spsr_fiq=200001d7 Before Violation, SW was in abort handler SP_abt=00000000, LR_abt=80832410, spsr_abt=200001d3 SCM FW: violation description Data Write Violation SCM FW Error Log: [Register Addr (32b)] = Err log value (32b) [0x48280000] = 0x00000000 [0x48280004] = 0x00000000 [0x48280008] = 0x00000000 [0x48280010] = 0x00400004 [0x48280014] = 0x00000000 [0x48280018] = 0xffffffff
FYI:
=> mmc list OMAP SD/MMC: 0 (SD) OMAP SD/MMC: 1 (eMMC) => mmc dev switch to partitions #0, OK mmc0 is current device => mmc info Device: OMAP SD/MMC Manufacturer ID: 3 OEM: 5344 Name: SD32G Bus Speed: 48000000 Mode: SD High Speed (50MHz) Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 29.7 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes => mmc dev 1 switch to partitions #0, OK mmc1(part 0) is current device => mmc info Device: OMAP SD/MMC Manufacturer ID: 13 OEM: 14e Name: S0J35 Bus Speed: 48000000 Mode: MMC High Speed (52MHz) Rd Block Len: 512 MMC version 5.1 High Capacity: Yes Capacity: 7.3 GiB Bus Width: 8-bit Erase Group Size: 512 KiB HC WP Group Size: 8 MiB User Capacity: 7.3 GiB WRREL Boot Capacity: 31.5 MiB ENH RPMB Capacity: 4 MiB ENH Boot area 0 is not write protected Boot area 1 is not write protected =>
Please help me in getting this solved.
Thank you