This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Graphic LCD Landscape to Portrait settings

Other Parts Discussed in Thread: AM1808

Hi,

I am using AM1808 with Sharp - LQ043T1DG01 tft Lcd 4.3 inch module. Now i am able to see the image in horizontal(LandScape ) view. I want to see all the applications and images in Vertical ( 
Portrait ) view.  

I used this in command line # echo 3 > /sys/class/graphics/fbcon/rotate_all

It rotates 270 degree angle of the existing image. Once the power OFF and ON it again start from Landscape. Can i have the settings or changes required in driver.

Please Any one can give your valuable suggestions.

Thanks 
Francis