Hi,
I would like to boot our TDA4VE based board of the eMMC UDA partition in filesystem mode -> using the same image as for the SD card!
If I set BOOTPINS accordingly I can see ROM booting from eMMC UDA partition but then the next stage is not booing correctly:
U-Boot SPL 2021.01-g2767b8f944 (Apr 14 2023 - 09:07:41 +0000) ti_sci system-controller@44083000: Message not acknowledgedSYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.0--v 08.06.00 (Chill Capybar') SPL initial stack usage: 13472 bytes Trying to boot from MMC1 init_env from device 17 not supported! Starting ATF on ARM64 core... ti_sci system-controller@44083000: ti_sci_get_response: Message receive failed. ret = -110 ti_sci system-controller@44083000: Message not acknowledgedFailed to put device 295 (-19) ### ERROR ### Please RESET the board ###
What am I missing?
Here is the content of FAT32 partition on the eMMC UDA partition:
=> fatls mmc 0:1 19016192 Image 78664 k3-am68-example-board.dtb 78664 oftree 411638 tiboot3.bin 970456 tispl.bin 1113036 u-boot.img 574 uEnv.txt 7 file(s), 0 dir(s) =>
Please note that I am not interested in "eMMC UDA partition RAW mode" nor in "eMMC boot0/boot1 booting"!