Hi,Ti Support Team
my customer plan to replace AM3352BZCZD60 by AM3352BZCZA100; i tell them it's ok,but customer need double check.
customer's question is as below;
Efore designer is checking the alternative part for AM3352BZCZD60.
Can you please kindly loop TI FAE in the mail for below questions.
if it is possible to run the AM3352BZCZA100 with exactly same MHz than we run the AM3352BZCZD60 (600 MHz). Usually that is the case with better and more expensive MCUs that they support higher MHz if needed, but they can as well run lower speed. But this is something which much be double checked. Then we also need a complete list of any other technical differences between the two.
If temperature rating and support for higher CPU frequency are the only difference, and if we can run the AM3352BZCZA100 at 600 MHz.