This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSLCDK6748: 20 to 14 pin converter

Part Number: TMDSLCDK6748

Hello we're using TMDSLCDK6748 board and we have XDS110 and XDS200, so but the board side JTAG has 14 pin and the debugger what we have is 20 pin, so we need to get the 20 to 14 pin converter.

and we were checking JTAG PIN CONVERTER - BH-ADP-20E_CTI-14T_TI (https://www.blackhawk-dsp.com/store/checkout/cart/configure/id/10316/) this converter and please confirm can we use this for connecting to the target board with standard TI 14-pin JTAG connector(pin 6 is keyed).

  • I'm not able to answer this question since you are asking about a product sold by Blackhawk. You should contact Blackhawk and request a schematic for the adapter they are selling and compare its connectivity to the TMDSLCDK6748 schematic to confirm it will connect the appropriate signals together.

    Regards,
    Paul