This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM - Daughter Board (Fusion Board) Cannot run Camera - LED D10 lit on Board

Part Number: TDA4VM


I Have attached Fusion board Rev C to my Common board . How ever when i power up board i can see Orange Light D10 lit on fusion board . Same time I am not able to run Single Camera Application
from Vision Apps . Can anybody tell me if it is Hardware issue ? And hoe can i resolve it ?/home/saurabh/Downloads/MicrosoftTeams-image.png

  • From picture - I see

    D5 (Green): OK, 3.3V rail

    D6 (Yellow): OK, 1.8V rail

    D7 (Green): OK, PGOOD LED

    D10 (Orange): OK, 5V rail

    How are you powering the Fusion board (are you using power cable between Common Processor and Fusion)?  Have you verified the dipswitches on EVM and Fusion board are set correctly for your application?  Are you getting an error message when you run application?

  • Hi Robert ,

    We are powering EVM board 12V 5A from Programmable power supply . Fusion Board is powered from Common Board to which it is attached with  -EXP PWR port.

    I have verified DIP switches on board and they are same as the one with working board.

    We tried running Single Camera Application from Vision Apps (SDK-8.04) Following is the Errors we are getting errors related to Deserializer write register

    root@j7-evm:/opt/vision_apps# ./run_app_single_cam.sh                           
    APP: Init ... !!!                                                               
    MEM: Init ... !!!                                                               
    MEM: Initialized DMA HEAP (fd=4) !!!                                            
    MEM: Init ... Done !!!                                                          
    IPC: Init ... !!!                                                               
    IPC: Init ... Done !!!                                                          
    REMOTE_SERVICE: Init ... !!!                                                    
    REMOTE_SERVICE: Init ... Done !!!                                               
       105.039429 s: GTC Frequency = 200 MHz                                        
    APP: Init ... Done !!!                                                          
       105.048058 s:  VX_ZONE_INIT:Enabled                                          
       105.048086 s:  VX_ZONE_ERROR:Enabled                                         
       105.048097 s:  VX_ZONE_WARNING:Enabled                                       
       105.050629 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!      
       105.052801 s:  VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for H!
    sensor_selection = [0]                                                          
    ldc_enable = [0]                                                                
    num_frames_to_run = [1000000000]                                                
    is_interactive = [1]                                                            
    IttCtrl_registerHandler: command echo registered at location 0                  
    IttCtrl_registerHandler: command iss_read_2a_params registered at location 1    
    IttCtrl_registerHandler: command iss_write_2a_params registered at location 2   
    IttCtrl_registerHandler: command iss_raw_save registered at location 3          
    IttCtrl_registerHandler: command iss_yuv_save registered at location 4          
    IttCtrl_registerHandler: command iss_read_sensor_reg registered at location 5   
    IttCtrl_registerHandler: command iss_write_sensor_reg registered at location 6  
    IttCtrl_registerHandler: command dev_ctrl registered at location 7              
    IttCtrl_registerHandler: command iss_send_dcc_file registered at location 8     
     NETWORK: Opened at IP Addr = 0.0.16.0, socket port=5000!!!                     
       105.065539 s: ISS: Enumerating sensors ... !!!                               
       105.065928 s: ISS: Enumerating sensors ... found 0 : DUMMY-UB953             
       105.065936 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS       
       105.065942 s: ISS: Enumerating sensors ... found 2 : UB96x_UYVY_TESTPATTERN  
       105.065947 s: ISS: Enumerating sensors ... found 3 : OV2311-UB953_LI         
       105.065952 s: ISS: Enumerating sensors ... found 4 : OV2311-UB933_MAGNA      
    Select camera port index 0-8 : 0                                                
    5 registered sensor drivers                                                     
    a : DUMMY-UB953                                                                 
    b : AR0233-UB953_MARS                                                           
    c : UB96x_UYVY_TESTPATTERN                                                      
    d : OV2311-UB953_LI                                                             
    e : OV2311-UB933_MAGNA                                                          
    Select a sensor above or press '0' to autodetect the sensor : Invalid selection 
    . Try again                                                                     
    5 registered sensor drivers                                                     
    a : DUMMY-UB953                                                                 
    b : AR0233-UB953_MARS                                                           
    c : UB96x_UYVY_TESTPATTERN                                                      
    d : OV2311-UB953_LI                                                             
    e : OV2311-UB933_MAGNA                                                          
    Select a sensor above or press '0' to autodetect the sensor : b                 
    Sensor selected : AR0233-UB953_MARS                                             
    LDC Selection Yes(1)/No(0) : LDC Selection Yes(1)/No(0) : 1                     
    Querying AR0233-UB953_MARS                                                      
       112.340663 s: ISS: Querying sensor [AR0233-UB953_MARS] ... !!!               
       112.341007 s: ISS: Querying sensor [AR0233-UB953_MARS] ... Done !!!          
       112.341017 s: ISS: Initializing sensor [AR0233-UB953_MARS], doing IM_SENSOR_!
       112.341311 s: ISS: Initializing sensor [AR0233-UB953_MARS], doing IM_SENSOR_!
       112.341934 s: ISS: ERROR: Initializing sensor [AR0233-UB953_MARS] failed !!! 
       112.341941 s: ISS: Initializing sensor [AR0233-UB953_MARS] ... Done !!!      
    Error initializing sensor AR0233-UB953_MARS                                     
    [MCU2_0]    112.341544 s: AR0233_Config ub960InstanceId=0 chId=0                
    [MCU2_0]    112.341720 s: Error writing 0x0 to UB960 register 0x1f              
    [MCU2_0]    112.341766 s:  UB960: Reg Write Failed for regAddr 1f               
    read_test_image_raw : Unable to open file /opt/vision_apps/test_data/img_test.rw
    app_create_viss : sensor_dcc_id = 233                                           
    Enabling LDC                                                                    
    Creating LDC                                                                    
       112.377112 s:  VX_ZONE_ERROR:[ownContextSendCmd:814] Command ack message ret1
       112.377134 s:  VX_ZONE_ERROR:[ownContextSendCmd:850] tivxEventWait() failed. 
       112.377140 s:  VX_ZONE_ERROR:[ownNodeKernelInit:538] Target kernel, TIVX_CMDg
       112.377146 s:  VX_ZONE_ERROR:[ownNodeKernelInit:539] Please be sure the targe
       112.377152 s:  VX_ZONE_ERROR:[ownNodeKernelInit:540] If the target callbacksl
       112.377309 s:  VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for no!
       112.377323 s:  VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed    
       112.377330 s:  VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed        
    Scaler is enabled                                                               
       112.380407 s: ISS: Starting sensor [AR0233-UB953_MARS] ... !!!               
    [MCU2_0]    112.376896 s:  VX_ZONE_ERROR:[tivxMutexLock:97] Mutex is NULL       
    [MCU2_0]    112.376966 s:  VX_ZONE_ERROR:[tivxVpacVissCreate:444] viss_aewb_locd
    [MCU2_0]    112.377567 s: ======================================================
    [MCU2_0]    112.377666 s:  Capture Status: Instance|0                           
    [MCU2_0]    112.377708 s: ======================================================
    [MCU2_0]    112.377756 s:  overflowCount: 0                                     
    [MCU2_0]    112.377793 s:  spuriousUdmaIntrCount: 0                             
    [MCU2_0]    112.377833 s:  frontFIFOOvflCount: 0                                
    [MCU2_0]    112.377869 s:  crcCount: 0                                          
    [MCU2_0]    112.377901 s:  eccCount: 0                                          
    [MCU2_0]    112.377935 s:  correctedEccCount: 0                                 
    [MCU2_0]    112.377972 s:  dataIdErrorCount: 0                                  
    [MCU2_0]    112.378008 s:  invalidAccessCount: 0                                
    [MCU2_0]    112.378046 s:  invalidSpCount: 0                                    
    [MCU2_0]    112.378086 s:  strmFIFOOvflCount[0]: 0                              
    [MCU2_0]    112.378119 s:  Channel Num | Frame Queue Count | Frame De-queue Cou|
    [MCU2_0]    112.378199 s:            0 |                 0 |                   |
    [MCU2_0]    112.379048 s: ======================================================
    [MCU2_0]    112.379141 s:  Capture Status: Instance|1                           
    [MCU2_0]    112.379180 s: ======================================================
    [MCU2_0]    112.379230 s:  overflowCount: 0                                     
    [MCU2_0]    112.379270 s:  spuriousUdmaIntrCount: 0                             
    [MCU2_0]    112.379308 s:  frontFIFOOvflCount: 0                                
    [MCU2_0]    112.379344 s:  crcCount: 0                                          
    [MCU2_0]    112.379376 s:  eccCount: 0                                          
    [MCU2_0]    112.379411 s:  correctedEccCount: 0                                 
    [MCU2_0]    112.379448 s:  dataIdErrorCount: 0                                  
    [MCU2_0]    112.379485 s:  invalidAccessCount: 0                                
    [MCU2_0]    112.379596 s:  invalidSpCount: 0                                    
    [MCU2_0]    112.379650 s:  strmFIFOOvflCount[0]: 0                              
    [MCU2_0]    112.379685 s:  Channel Num | Frame Queue Count | Frame De-queue Cou|
                                                                                    
                                                                                    
     ==========================                                                     
     Demo : Single Camera w/ 2A                                                     
     ==========================                                                     
                                                                                    
     p: Print performance statistics                                                
                                                                                    
     s: Save Sensor RAW, VISS Output and H3A output images to File System           
                                                                                    
     e: Export performance statistics                                               
                                                                                    
     u: Update DCC from File System                                                 
                                                                                    
                                                                                    
     x: Exit                                                                        
                                                                                    
     Enter Choice:                                                                  
    Unsupported command                                                             
                                                                                    
                                                                                    
                                                                                    
     ==========================                                                     
     Demo : Single Camera w/ 2A                                                     
     ==========================                                                     
                                                                                    
     p: Print performance statistics                                                
                                                                                    
     s: Save Sensor RAW, VISS Output and H3A output images to File System           
                                                                                    
     e: Export performance statistics                                               
                                                                                    
     u: Update DCC from File System                                                 
                                                                                    
                                                                                    
     x: Exit                                                                        
                                                                                    
     Enter Choice:    112.381767 s: ISS: Starting sensor [AR0233-UB953_MARS] failed!
    Failed to start sensor AR0233-UB953_MARS                                        
    Defaulting to file test mode                                                    
    [MCU2_0]    112.381191 s: AR0233_StreamOn: chId = 0                             
    get_dcc_dir_size : Could not open directory or directory is empty /opt/vision_a
    

  • Mentioned DIP switch settings on board match working board.  Do you have a working Fusion setup and a non-working Fusion setup?  If so - did you see different LEDs illuminate (was that the point of your original question)?