Dear All,
I want to use the C6747 EVM to send AT commands to a GSM evaluation board. The GSM board has a RS232 interface attached to a USB port. I can send AT commands from the PC to the GSM board using hyperterminal because I have the drivers for Windows. However, when I connect the GSM board to the C6747 USB port and run the biosusb keyboard hid dev example I get the following output:
uhub0: 2 ports with 2 removable, self powered
uhub0: new device port=1 depth=1 speed=full
ucompdev0 FTDI Dual RS232, class 0/0, rev 2.00/5.00, addr 2
unknown2: at uhub0 port 1 (addr 2) connected. No driver was found for this device.
Is there any RS232 driver or source code available that I could use to be able to send AT commands over the USB?
I look forward to hearing from you!
Best regards,
Bogdan