Part Number: AM4372
HI,.
A customer of ours has asked about the ADC circuitry of the AM4372.
They are looking at Figure 12-4. in TRM.
ADC1_0/2/4/6 are connected to analog voltage input and adc1_1/3/5/7 to GND, but they are concerned about the effect of leakage current at this time.
(1) What is the resistance tolerance of the 9kΩ resistor in the differential line?
(2) The bottom of the figure states "The differential input impedance of each preamplifier is 18 kohms biased to VDDA_ADC1 divided by 2 with a 22k-50k ohm source.
Can I assume that the Bias Supply in Figure 12-4. is a circuit in which VDA_ADC1 is divided by 2 with a 22k-50k resistor?
Best Regards,
Kouji Nishigata