Other Parts Discussed in Thread: AM3517, MSP430F5528, TS3USB30, TS3USB221
Hello,
Due to the nature of my design I am interfacing the MSP430F5528 to the AM3517. Can I connect both USB lineof MSP430F5528 and the AM3517 OTG (USB0_VBUS, USB0_DP, USB0_DM and USB0_ID) together and having it externally available as a one set DP, DM, GND and the VBUS. When the PC is interfaced through USB with the unit by software to decide which processor to communicate to the host (MSP430F5528 or AM3517). My thought was that to enable one USB port at a time and disable the other. This is possible for the MSP430F5528 since its USB data lines are multiplex with the I/O lines but I am not sure if this is true in regard to AM3517.
Thank you,
Ali.
Maximum
rON = 0.2