Hello all,
I want to configure the ipipe demo which come with
DM355SDK783911.
I am using DM355 LeopardBoard which is using OV7725
image sensor.
I have few doubts/questions:
1.In the board
prompt when i do ls -l /dev i am getting the following output.
crwxr-xr-x 1 root root 249, 0 Jan 1 00:00
cmem
crw-rw---- 1 root root 5, 1
Jan 1 00:00 console
crw-rw---- 1 root
root 116, 0 Jan 1 00:00 controlC0
crw-rw---- 1 root root 10, 63 Jan 1 00:00
cpu_dma_latency
drwxr-xr-x 2 root root 100
Jan 1 00:00 fb
crw-rw---- 1 root
root 29, 0 Jan 1 00:00 fb0
crw-rw---- 1 root root 29, 1 Jan 1 00:00
fb1
crw-rw---- 1 root root 29, 2
Jan 1 00:00 fb2
crw-rw---- 1 root
root 29, 3 Jan 1 00:00 fb3
crw-rw---- 1 root root 1, 7 Jan 1 00:00
full
drwxr-xr-x 2 root root 40
Jan 1 00:00 i2c
crw-rw---- 1 root
root 89, 1 Jan 1 00:00 i2c-1
drwxr-xr-x 2 root root 40 Jan 1 00:00
input
crw-rw---- 1 root root 1, 2
Jan 1 00:00 kmem
crw-rw---- 1 root
root 1, 11 Jan 1 00:00 kmsg
srw-rw-rw- 1 root root 0 Jan 1 00:00
log
brw-rw---- 1 root root 7, 0
Jan 1 00:00 loop0
brw-rw---- 1 root
root 7, 1 Jan 1 00:00 loop1
brw-rw---- 1 root root 7, 2 Jan 1 00:00
loop2
brw-rw---- 1 root root 7, 3
Jan 1 00:00 loop3
brw-rw---- 1 root
root 7, 4 Jan 1 00:00 loop4
brw-rw---- 1 root root 7, 5 Jan 1 00:00
loop5
brw-rw---- 1 root root 7, 6
Jan 1 00:00 loop6
brw-rw---- 1 root
root 7, 7 Jan 1 00:00 loop7
crw-rw---- 1 root root 1, 1 Jan 1 00:00
mem
crw-rw---- 1 root root 10, 62
Jan 1 00:00 network_latency
crw-rw---- 1 root
root 10, 61 Jan 1 00:00 network_throughput
crw-rw---- 1 root root 1, 3 Jan 1 00:00
null
crw-rw---- 1 root root 116, 24
Jan 1 00:00 pcmC0D0c
crw-rw---- 1 root
root 116, 16 Jan 1 00:00 pcmC0D0p
crw-rw---- 1 root root 5, 2 Jan 1 00:00
ptmx
drwxr-xr-x 2 root root 0
Jan 1 00:00 pts
brw-rw---- 1 root
root 1, 0 Jan 1 00:00 ram0
crw-rw---- 1 root root 1, 8 Jan 1 00:00
random
drwxr-xr-x 2 root root 120
Jan 1 00:00 snd
crw-rw---- 1 root
root 116, 33 Jan 1 00:00 timer
crw-rw---- 1 root root 5, 0 Jan 1 00:00
tty
crw-rw---- 1 root root 4, 64
Jan 1 00:00 ttyS0
crw-rw---- 1 root
root 4, 65 Jan 1 00:00 ttyS1
crw-rw---- 1 root root 4, 66 Jan 1 00:00
ttyS2
crw-rw---- 1 root root 1, 9
Jan 1 00:00 urandom
crw-rw---- 1 root
root 189, 0 Jan 1 00:00 usbdev1.1
crw-rw---- 1 root root 253, 1 Jan 1 00:00
usbdev1.1_ep00
crw-rw---- 1 root root 253, 0
Jan 1 00:00 usbdev1.1_ep81
crw-rw---- 1 root
root 81, 0 Jan 1 00:00 video0
crw-rw---- 1 root root 81, 1 Jan 1 00:00
video2
crw-rw---- 1 root root 81, 2
Jan 1 00:00 video3
crw-rw---- 1 root
root 10, 130 Jan 1 00:00 watchdog
crw-rw---- 1 root root 1, 5 Jan 1 00:00 zero
But
the above driver list doesn;t contain dm355_ipipe driver.
Do we
have to manually ran application to generate .ko file and install the
dm355_ipipe driver.
If anyone knows the procedure.If there is any demo or example which i can run to do this.
Also i am trying to compile the
ipipe demo but i think the excutable also uses dm355_ipipe driver.
Does
ipipe demo require any other drivers installed.
Thanks and
Regards,
Mayank