Part Number: AM623
Other Parts Discussed in Thread: SYSCONFIG
My customer has a couple of question on the PMIC and the supply rails.
1. Power supply of MMC1 / SDIO interface (VDDSHV5_MMC1): Can it be connected to DVDD1V8 (VDDSHVy) in our use case?
I assume not but would like to get confirmation.
2. Can VDDA_3P3_USB be connected to VDD_3V3 or USB_VBUS (=3V3)?
I assume not but would like to get confirmation.
3. The PMIC (TPS6521902) already has PowerGood detection. So what would be the advantage of using power supply monitoring by CPU?
In their case only the 3.3V is directly supplied and not going through the PMIC therefore I guess that is the only one they would monitor using VMON
4. In SysConfig only 1 voltage (1.8 or 3.3V) for both of them can be selected for signals PMIC_LPM_EN0 (VDDSHV_CANUART) and WKUP_CLKOUT0 (VDDSHV_MCU). Are VDDSHV_CANUART and VDDSHV_MCU connected?
5. USB will only be used with 3V3 --> Do we have to connect VDDA_1P8_USB nevertheless? --> to 1V8 or 3V3?
In SysConfig there is only one voltage to be selected (currently 3V3 selected). According to the e2e and if USB operation is desired, all related signals/rails must be connected as per the datasheet regardless of interface type (USB1.1/USB2.0). Please see Table 6-74 and Section 7.4 of the device datasheet for more information. Can you please confirm if they need to connect to 1.8V or 3.3V?
6. We will supply USB_VBUS (=3V3) externally --> any recommendations on this? Or what about connect USB VBUS to VDD_3V3?
So they will not implement the circuit as described in datasheet 9.2.3. (They know: not being compatible to USB Spec.); The range is 0...3,465 V. BSH is owning the USB_VBUS supply and are supplying it externally with 3.3V. So do they still need the Zener diode to be used to support up to 20V.
BR,
Frank