This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: If CSI is not used but boundary scan is what to do with W13, W14?

Part Number: AM623


"If CSIRX0 is not used and the device boundary scan function is required, each of these balls must be connected to valid power sources." (refered to table 6-74. in datasheet) . Can you please confirm that W13, W14 must be tied to VSS?

Best regards,

Frank