This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: SBL eMMC boot failed

Part Number: PROCESSOR-SDK-J721E

Hi Ti,

When we are debugging SBL eMMC BOOT0 startup, tifs.bin and app are obtained from the UDA BOOT partition of EMMC,which dose not match with PDK user guide chapter:  5.2.8.3. Booting Via eMMC BOOT0 partition we confirmed with FAE of TI China, this may be a bug.  Could you confirm that?

On PDK user guide, chapter 5.3. Boot App, it only support OSPI and MMCSD. Is there a plan or a patch we could apply to enable boot app loading image from eMMC?

Thanks

  • And the boot err, how to fix it ?

    NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
    NOTICE: BL31: Built : 22:56:45, Mar 3 2023


    ERROR: GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader

    I/TC:
    I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Fri Mar 3 22:59:24 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
    I/TC: Primary CPU initializing

  • Hi,

    When we are debugging SBL eMMC BOOT0 startup, tifs.bin and app are obtained from the UDA BOOT partition of EMMC,which dose not match with PDK user guide chapter:  5.2.8.3. Booting Via eMMC BOOT0 partition we confirmed with FAE of TI China, this may be a bug.  Could you confirm that?

    Are you trying to boot the SBL from boot0 partition and the app and tifs from UDA?

    Regards,
    Parth