This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Increasing IRAM size in the Audio SOC example (DSP code on the OMAP L138)

I'm using the Audio SOC example provided in the SDK as a template for my own application. Since I'm using quite a few large data buffers (on the DSP side), I want to place all data in L2 memory instead of external memory to increase the speed. Thus, I have added the following lines to the file "audio.tcf" :

// Increase size of IRAM (L2 memory) to 224kB

var IRAM = prog.module("MEM").instance("IRAM");

IRAM.len = 0x38000; // 224kB

which builds without problems and the .map-file looks OK (to me), see memory configuration below :

         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------
  IRAM                  11800000   00038000  00013144  00024ebc  RWIX
  CACHE_L2              11838000   00008000  00000000  00008000  RWIX
  CACHE_L1P             11e00000   00008000  00000000  00008000  RWIX
  CACHE_L1D             11f00000   00008000  00000000  00008000  RWIX
  L3_CBA_RAM            80000000   00020000  00000000  00020000  RWIX
  RESET_VECTOR          c3e00000   00000080  00000000  00000080  RWIX
  DDR                   c3e00080   000fff80  00094fdf  0006afa1  RWIX
  DSPLINKMEM            c3f00000   00030000  00000000  00030000  RWIX
  POOLMEM               c3f30000   000d0000  00000000  000d0000  RWIX

However, when I start to actually place data in IRAM I run into weird problems (which does not ocurr with the data in external memory - then everything is fine but slow). Is the above procedure for increasing the IRAM size OK, or should I do something else? Have I missed something?

Thanks in advance!