This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: DSS output resolution

Part Number: AM625

Hello,

Let me confirm about below.

* According to TRM, there is following description.

*Support for up to 4K-pixels wide frame buffer for 8/16/32/64-bit per pixel, if the frame buffer is used without scaling (that is, no upscale/downscale) in the video pipelines.

If user do not perform scaling in this device, I understood there is possiblity to output 4K-pixels.
However, on the other hand, there is following description.

*Support for up to 2560-pixels wide frame buffer for 8/16-bit per pixel, if scaling is enabled in video pipelines

I would like you to confirm available width and height if user do not use frame buffer for scaling.
Could you please tell me acceptable width and height case of "4K-pixels" ?
(According to TRM, it seems maximum line buffer is 4096. so this device can accept over general 4K-pixel 3840, but I'm not sure spec for frame buffer..)

BR,