Part Number: AM623
Dear Champs,
My customer has a trouble to boot-up their custom board using SD card. The issue is that kernel copy failed in some SD card with below log whereas there is no issue in other SD card.

In their customer board, AM6231 GP device(AM6232ATCGGAALW) was used and they are using Linux SDKv8.6.0.
Do you think this issue caused by default setting for HSFS device in Linux SDKv8.6.0 and this issue can be resolved when below patch will be applied?
booting was success in below SD card,
* Samsung EVO 32
Boot failed SD card.
* Samsung EVO+ 32
* Sandisk Industrial 32GB, 8GB
Thanks and Best Regards,
SI.