This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VPSS Capture specifications/limitations

We are in the process of selecting a cpu for our next gen platform and got a question about the video capture capability of DM8168. I understand that the the VPSS sub system runs on a separate mcu and has its own closed firmware.

1- Is there still an hardware interface for programming the capture ? Using registers and handling interrupts and dma ourselves ?

2- Is OMX library the only software available for handling the capture?

3- Does custom resolution/framerate are supported ? ie 2048x2048@10Hz or 640x480@120Hz or maybe something odd like 1024x120@30fps ?

Regards,

Pierre-Olivier