This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H12: How to modify the linux code to support memblock=debug

Genius 13655 points

Part Number: 66AK2H12

Hello Champs,

HW: TI66ak  EVM board
SW: ti-processor-sdk-linux-k2hk-evm-06.00.00.07 (linux kernel version 4.19.38)

1. In u-boot bootargs: adding memblock=debug, earlycon=uart8250,mmio32,0x02530c00, 115200n8,then booting the OS, the console prompted: Memory policy: Da. ta cache writealloc. arm PC entered to exception, data abort, PC is 0xffff_000C


2. If not modifying the bootargs, the OS can boot successfully. 


How to modify the linux code to support memblock=debug? 

Thanks
Regards
Shine