Hi Ti Ethernet experts,
My customer is enabling J721e CPSW9g Native Ethernet mode by applying “k3-j721e-quad-port-eth-exp.dtbo”. Then he got 4 eth on J721e with Quad-Port Ethernet Expansion board. The 4 eth are all up. But he cannot ping on eth 4 in CPSW9G native ethernet mode.
BTW, the CPSW2g is also in Native Ethernet mode, and it can ping.
The following shows the stage results he got:
- enabled J721e CPSW9g Native Ethernet mode, add env in uboot uEnv.txt:
- Eth4 is on VSC8514 is link up
But cannot ping PC using eth4 with CPSW9G, no packets received.
The tcpdump on the eth4 shows below, there is no packets received when pc ping the board. But the link status showing “yes”
But with the same steps the eth0 of CPSW2G can be pinged and packets can be received successfully.
Could you please provide some feedback on this question, it seems the status shows the eth4 in CPSW9G native ethernet mode is connected correctly, but why there is no packets received?
Thank you so much!
Kevin