Part Number: PROCESSOR-SDK-AM62X
Hello,
I would like to try full sdk build based on bitbake.
At first, I tried to set HDD size definition is 256GB.
However, I got error for size when I performed full SDK build.
It is not for AM62, but I found following information on other device SDK.
https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-j7200/08_06_00_11/exports/docs/j7200/linux/Overview_Building_the_SDK.html
The build will ~250GB of hard disk space for building the tisdk-default-image.
From above, I assume that I need more HDD size than 256GB for full SDK build, however if you have recommended HDD size information for following usecase which is described in SDK web documentation each other ?
tisdk-core-bundle : For full SDK
tisdk-default-image : For target filesystem
tisdk-base-image : For minimal target filesystem
meta-toolchain-arago-tisdk : Devkit
BR,