This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: Unable to boot from SD card

Part Number: SK-AM62

I received the board SK-AM62 (E3A) and I am unable to boot.

I've flashed two different SD cards (8GB, 32GB) with the image inside "tisdk-default-image-am62xx-evm.wic.xz" using Balena Etcher on Windows and Ubuntu Linux.

I have tried 3 different Micro-USB cables for UART (J15).

I have tried 3 different PSU's that can provide up to 15V 3A.

I have tried 3 different USB-C cables (Type-C PWR, J11)

I have reconfigured the DIP switches in all TI Doc specified Boot Modes, both as specified by the TI docs, and by inverting them (just in case).

I have tried connecting UART first, then USB-C, and vice versa.

LEDs light up (LD13, LD16, LD10, LD17

I have tried PuTTY and Tera Term, both give me blank output (COM3 (first COM of the 4 listed), 115200, etc... as specified by docs)

I have followed the TI docs in detail.

What else can I do?