Part Number: SK-AM62
Dear TI Expert,
HW : AM62x SK-EVM
SW : Processor SDK 8.5, MCU SDK 8.5
I'm trying to replace R5 firmware binary with new one I built.(examples/drivers/ipc/ipc_rpmsg_echo_linux/am62x-sk/r5fss0-0_freertos)
I created new tispl.bin as following steps.
1). Build R5 fw example
jwook@jwook-Desktop:~/ti/workspace_v12/ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang/Release$ ll total 3320 drwxrwxr-x 3 jwook jwook 4096 5월 3 11:40 ./ drwxrwxr-x 6 jwook jwook 4096 5월 3 11:11 ../ -rw-rw-r-- 1 jwook jwook 267656 5월 3 11:40 am62-mcu-r5f0_0-fw -rw-rw-r-- 1 jwook jwook 665 5월 3 11:40 ccsObjs.opt -rw-rw-r-- 1 jwook jwook 7511 5월 3 11:40 ipc_rpmsg_echo.d -rw-rw-r-- 1 jwook jwook 145436 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang.appimage -rw-rw-r-- 1 jwook jwook 52 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang.appimage_xip -rw-rw-r-- 1 jwook jwook 1040966 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang_linkInfo.xml -rw-rw-r-- 1 jwook jwook 1340476 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang.out -rw-rw-r-- 1 jwook jwook 145404 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang.rprc -rw-rw-r-- 1 jwook jwook 20 5월 3 11:40 ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang.rprc_xip -rw-rw-r-- 1 jwook jwook 337427 5월 3 11:40 ipc_rpmsg_echo_linux.Release.map -rw-rw-r-- 1 jwook jwook 15256 5월 3 11:40 ipc_rpmsg_echo.o -rw-rw-r-- 1 jwook jwook 9864 5월 3 11:40 main.d -rw-rw-r-- 1 jwook jwook 6148 5월 3 11:40 main.o -rw-rw-r-- 1 jwook jwook 6500 5월 3 11:40 makefile -rw-rw-r-- 1 jwook jwook 668 5월 3 11:40 objects.mk -rw-rw-r-- 1 jwook jwook 2205 5월 3 11:40 sources.mk -rw-rw-r-- 1 jwook jwook 3601 5월 3 11:40 subdir_rules.mk -rw-rw-r-- 1 jwook jwook 2932 5월 3 11:40 subdir_vars.mk drwxrwxr-x 2 jwook jwook 4096 5월 3 11:40 syscfg/ -rw-rw-r-- 1 jwook jwook 9059 5월 3 11:40 temp_stdout_Release.txt
2). R5 firmware file copy
I copied the "am62-mcu-r5f0_0-fw" file because there was no "ipc_echo_testb_freertos_mcu1_0_release.xer5f" file in Release directory, but I'm not sure if this is correct.
cp ~/ti/workspace_v12/ipc_rpmsg_echo_linux_am62x-sk_r5fss0-0_freertos_ti-arm-clang/Release/am62-mcu-r5f0_0-fw <path_to_linux_installer>/board-support/prebuilt-images/ipc_echo_testb_mcu1_0_release_strip.xer5f
3). Build u-boot
make u-boot
4). Flash tispl.bin and u-boot.img
If I try booting after flashing in the above step, device is stuck at the log as shown below.
NOTICE: BL31: v2.7(release):v2.7.0-359-g1309c6c805-dirty NOTICE: BL31: Built : 11:48:12, Dec 14 2022 I/TC: I/TC: OP-TEE version: 3.19.0-15-gd6c5d0037 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Wed Dec 14 11:52:03 UTC 2022 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot
Please correct me If i'm wrong. or Please let me know how to replace R5 firmware with new one.
Thanks&Regards,
Jaewook