Part Number: AM623
Other Parts Discussed in Thread: AM625-Q1, AM625,
Hi TI
In TRM, it mentioned the maximum output resolution will be limited with BT.1120 progressive mode.
How about the maximum output resolution and frame rate when we use BT.1120?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Austin.chen
Thank you for the query.
Please refer attached.
Note: Link deleted.
Regards,
Sreenivasa
Hello Austin.chen
Thank you for the note.
Please refer below.
AM625-Q1 supports DPI. Can it output YUV? Or only RGB?
We only support the following:
Parallel MIPI DPI 2.0 (Digital Pixel Interface): RGB 16/18/24-bit output with separate sync signals
BT.656/BT.1120 interface: YUV422 output (8/10-bit modes) with embedded syncs
Regards,
Sreenivasa
Since the maximum pixel clock is only 165MHz, can we expect to have 1920x1080 @30fps while using BT.1120 progressive mode?
Also AM623 dosn't include GPU, can AM623 have the same video output cability as AM625?
Hello Austin.chen
Thank you for the inputs.
Since the maximum pixel clock is only 165MHz, can we expect to have 1920x1080 @30fps while using BT.1120 progressive mode?
Lat me check internally.
AM623 dosn't include GPU, can AM623 have the same video output cability as AM625?
Can you please start a new thread. I can assign this to the experts, and this would help wider E2E users.
Regards,
Sreenivasa
Hello Austin.chen
Since the maximum pixel clock is only 165MHz, can we expect to have 1920x1080 @30fps while using BT.1120 progressive mode?
Lat me check internally.
I did a quick check with the software designer and received the input that this should be feasible. Please note that this has not been verified or tested.
I will update the thread if i have some additional inputs.
Regards,
Sreenivasa