Reading this FAQ on the logic site:
http://www.logicpd.com/product-support/frequently-asked-questions-faq/what-difference-between-am1808-som-m1-included-kits-a
I discovered that the AM1808 SOM modules sold with the EVM and Experimenter kits have additional power measurement circuitry added to the PCB which seems to be wired to J13 PMDC Connector on the EVM.
We searched all Locig and Texas websites but were unable to find any board or adapter meant to connect to J13 to read those power signals.
The only board we found is this Wattson Breakout Board:
http://createnewstuff.webs.com/breakoutboardwattson.htm
So here comes the questions:
1. Is that Wattson Breakout Board sold on Createnewstuff.com an official (or at least supported) Texas/Logic board?
2. If not, is it possible to buy an official power measurement board for AM1808 EVM SOM ?
3. Is there any way to download the Logic Wattson software mentioned on the above page for evaluation without registration (which requires a DM3730 Torpedo Serial Number?)
Best regards, Gabriele.