Other Parts Discussed in Thread: TMS320C6672, CDCE62005
In the EVM Board document for TI, for the Clock Diagram, it can be seen that the frequency for the various clock input are as follows:
a. core clk: 100MHz
b. SRIO/ SGMII clk: 312.5MHz
c. DDR clk: 66.7MHz
d. PCIe clk: 100MHz
e. Hyperlink: 312.5MHz
f. PASS: 100MHz
May I know the reason for these frequencies? Is it randomly assigned or is there special frequencies that each clk can take.