Hi,
I am having problems getting USB to work in u-boot with the OMAP3530 and TPS65950. We are using the OTG in 'host' mode to use a USB flash storage device for running Linux. We are finding that the VBUS signal is only reaching a level of 1.5V - no where near the required 5V for USB. Does anyone have any ideas as to why this may be?
We have noticed that the OMAO3530 EVM uses an external OTG transceiver, instead of the one as part of the TPS65950 device. I can confirm that USB works using the EVM running the same u-boot software. Is there a particular reason why the TPS65950 is not used as an OTG transceiver?
Thanks
Andy