This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6 Integra questions - ET1011c 1 obsolete

Here are some Integra questions:

  1. Can I leave off all power connections on the analog video output section (page 9 on the EVM schematic) since it is not needed?
  2. Since I am not using SATA or PCIe, can I leave off all of the power connections on page 16 of the EVM that power those sections?  

The ET1011C 1 Gbit Ethernet PHY used on the EVM is obsolete.  Can you confirm that a Marvell 88E1111-B2-RCJ1C000 is compatible with the driver software on the EVM?  If not, can you recommend other compatible PHYs