Part Number: LINUXSDK-OMAPL138
Other Parts Discussed in Thread: TMS320C6748
Hi,
I am using TMS320C6748 DSP development kit (LCDK). I want to interface DDR2-RAM (MT47H64M16NF-25E AIT:M).
The maximum frequency input to the DDR2 controller is 312MHz at 1.3V NOM Operating voltage. Hence the Maximum frequency of DDR_CLK is 156MHz at 1.3V.
But the PLL operating frequency range is 300MHz to 600MHz. So can I increase the PLL1 frequency from 312MHz to 456MHz?