Hi,.
We have a question from one of our customers about the setting of CPSW_SL_MACCTRL in Ethernet Subsystem.
What are the IFCTL_A and IFCTL_B settings for Bit[15,16] respectively?
AM437x has 2 ports of EMAC, do you set the transmission rate of RMII (RMII0,RMII1) for each port?
The same question is posted for AM335x in the following forum thread (I believe AM437x is basically the same).
Here it is stated that IFCTL_B is not required, but is the RMII transmission rate not set on a per-port basis, but only determined by IFCTL_A?
If so, is it not possible to change the RMII rate on port1 and 2?
AM335x CPGMAC_SL MAC CONTROL REGISTER - Processors forum - Processors - TI E2E support forums
Best Regards,
Kouji Nishigata