This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AAC-LC encoder configuration...

Hello...

I’m using AAC-LC encoder in DM368.

According to a playing test, it has no problem with ordinary players. (fileformat : .mp4)

But, it has a lagging sound problem with VLC only.
In addition, Samsung Galaxy S2 smart phone has same problem as VLC.

I want to use as AAC-LC, 1 channel, 8khz, 24kbps, 16bit

Please check the following configuration and let me know any changing required.


   ittiam_params.aud_params.size   = sizeof(ITTIAM_EAACPLUSENC_Params);
   ittiam_params.aud_params.sampleRate  = 8000;
   ittiam_params.aud_params.bitRate = 24000;
   ittiam_params.aud_params.channelMode = IAUDIO_1_0;
   ittiam_params.aud_params.dataEndianness = XDM_LE_16;
   ittiam_params.aud_params.encMode = IAUDIO_CBR;
   ittiam_params.aud_params.inputFormat = IAUDIO_INTERLEAVED;
   ittiam_params.aud_params.inputBitsPerSample = 16;
   ittiam_params.aud_params.maxBitRate = 256000;
   ittiam_params.aud_params.dualMonoMode = IAUDIO_DUALMONO_LR;
   ittiam_params.aud_params.crcFlag = XDAS_FALSE;
   ittiam_params.aud_params.ancFlag = XDAS_FALSE;
   ittiam_params.aud_params.lfeFlag = XDAS_FALSE;
   ittiam_params.noChannels = 1;
   ittiam_params.aacClassic = 1;
   ittiam_params.psEnable = 0;
   ittiam_params.dualMono = 0;
   ittiam_params.downmix = 0;
   ittiam_params.useSpeechConfig = 0;
   ittiam_params.fNoStereoPreprocessing = 0;
   ittiam_params.invQuant = 2;
   ittiam_params.useTns = 1;
   ittiam_params.use_ADTS = 0;
   ittiam_params.use_ADIF = 0;
   ittiam_params.full_bandwidth = 0;
   ittiam_params.i_channels_mask = 0;
   ittiam_params.i_num_coupling_chan = 0;
   ittiam_params.write_program_config_element = 0;