Other Parts Discussed in Thread: DA8XX
Hello All,
We are using kernel 3.2 on Phycore AM335x SOM. The AM3354 processor is used on the SOM.
We are trying to upgrade the Linux kernel to kernel version 3.10. Some how the kernel hangs at startup after upgrading it. Below are the logs for quick reference.
barebox 2013.07.0 #1 Thu Oct 13 10:22:44 CDT 2022
Board: Phytec phyCORE-AM335x
omap-hsmmc omap4-hsmmc0: registered as omap4-hsmmc0
mci0: registered disk0
cpsw cpsw0: detected phy mask 0x1f
mdio_bus: miibus0: probed
eth0: got preset MAC address: EC:24:B8:7A:B0:ED
I2C probe
i2c-omap i2c-am33xx0: bus 0 rev0.11 at 100 kHz
probe buswidth
nand: ONFI param page 0 valid
nand: ONFI flash detected ...
nand: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron MT29F8G08ADADAH4), page size: 2048, OOB size: 64
malloc space: 0x85ff4000 -> 0x87ff3fff (size 32 MiB)
running /env/bin/init...
addpart: No such file or directory
Hit m for menu or any other key to stop autoboot: 0
booting nand...
Loading OS arm Linux zImage '/dev/nand0.kernel.bb'
commandline: console=ttyO3,115200 ip=none root=ubi0:root ubi.mtd=nand0.root,2048 rootfstype=ubifs da8xx_fb.panel_name=G065VN01_V2 mtdparts=om)
arch_number: 4144
Could you please guide us on this issue?
What are the minimum required changes we should do to successfully boot with the Linux kernel 3.10 and get the console?
Thanks,
Prathamesh Kulkarni