This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM6x: Ethercat Master using Linux

Other Parts Discussed in Thread: PROCESSOR-SDK-AM64X, PROCESSOR-SDK-AM62X

PROCESSOR-SDK-AM64X

PROCESSOR-SDK-AM62X

Hi TI Expert, 

Question1: Is there any  open source code to recommend for EtherCAT MainDevice  in Linux ?

Answer:

There is an constrained open source EtherCAT MainDevice at https://etherlab.org/en/ethercat/ and https://github.com/OpenEtherCATsociety/SOEM .

We would not recommend these for multiple reasons, including feature set and incompatibility with Linux upstream. But with a significant development team owning the implementation at the customer they can make sense.

See https://www.acontis.com/en/ethercat-master-options-ec-master-vs-open-source-etherlab-SOEM.html for a overview of the open source EtherCAT solutions  compared to a commercial EtherCAT MainDevice solution.

Question2: Do we really need a third party for this ?  

Answer:

Yes. We recommend looking at the following solutions 

Question3: Does TI have  a demo on TI AM64 family for both EtherCat MainDevice and SubDevice configurations ?

Answer:

Please refer below sections:

Note:

1. Customer can take IgH or Simple Open EtherCAT Master (SOEM) for free. TI does not directly support this so requires customers to invest in SW and updates etc.

2. On AM64 with the on chip Cortex R5 cores, IBV offers the lowest latency stack based on R5

3. Acontis Linux stack is very competitive on latency. 

Thanks