Part Number: SK-AM62A-LP
Hi, I used SK-AM62A-LP with ubunto.
I want to connect the CSI-2 camera to the EVM board.
I chose this camera. (Arducam ToF Camera / Device Code : UC-981)
After connecting the camera to the CSI-2 port, the EVM board was activated in boot mode.
I checked the list of connected cameras using the following command, but no connected cameras were found.
root@am62axx-evm:/opt/edgeai-gst-apps# v4l2-ctl --list-devices
TI-CSI2RX (platform:30102000.ticsi2rx):
/dev/media0
wave5-dec (platform:wave5-dec):
/dev/video0
wave5-enc (platform:wave5-enc):
/dev/video1
Can't I operate it on the SK-AM62A-LP board with the camera presented above?
If this camera and the EVM board are not compatible, could you recommend another camera?