This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4x - CPSW9g static IP configuration

Part Number: TDA4VM

Hello,

We are experiencing some difficulties regarding CPSW9g static IP configuration and connection.

Our setup:

1. PC (Windows) Ethernet -> TDA4 Ethernet (CPSW9g port)

2. Using PSDK 8.02 version

When using DHCP (ETHAPP_LWIP_USE_DHCP (1)) everything is working as expected. In that case we can ping our PC.

But when we try to set static IP configuration we can't ping PC.

We also came across this post: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1124677/tda4vm-ping-a72-qnx-from-pc-through-cpsw9g-with-static-ip

"-2- The released EthFW code implement support for getting dynamic IP address from DHCP server. Support for Static IP address require updates to the EthFW code. Has this been taken care in EthFW?"

The changes we did are under vision_apps/utils/ethfw/src/app_ethfw_freertos.c :

/* DHCP or static IP */
#define ETHAPP_LWIP_USE_DHCP            (0)
#if !ETHAPP_LWIP_USE_DHCP
#define ETHFW_SERVER_IPADDR(addr)       IP4_ADDR((addr), 192,168,1,200)
#define ETHFW_SERVER_GW(addr)           IP4_ADDR((addr), 192,168,1,1)
#define ETHFW_SERVER_NETMASK(addr)      IP4_ADDR((addr), 255,255,255,0)
#endif

1. On PC side we have set static IP -> 192.168.1.13

2. On TDA4 side for eth1 (CPSW9G) we also set static IP -> 192.168.1.20

dl-eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500  metric 1
        inet 192.168.1.20  netmask 255.255.255.0  broadcast 192.168.1.255
        inet6 fe80::72ff:76ff:fe1d:92c2  prefixlen 64  scopeid 0x20<link>
        ether 70:ff:76:1d:92:c2  txqueuelen 1000  (Ethernet)
        RX packets 24  bytes 2106 (2.0 KiB)
        RX errors 0  dropped 3  overruns 0  frame 0
        TX packets 31  bytes 3808 (3.7 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

Here is the log from vision_apps_init.sh:

root@TTX-PM300-00001:/opt/vision_apps# ./vision_apps_init.sh
root@TTX-PM300-00001:/opt/vision_apps# [MCU2_0]     88.284601 s: CIO: Init ... Done !!!
[MCU2_0]     88.284679 s: ### CPU Frequency = 1000000000 Hz
[MCU2_0]     88.284723 s: APP: Init ... !!!
[MCU2_0]     88.284748 s: SCICLIENT: Init ... !!!
[MCU2_0]     88.285016 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[MCU2_0]     88.285066 s: SCICLIENT: DMSC FW revision 0x8
[MCU2_0]     88.285117 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0]     88.285157 s: SCICLIENT: Init ... Done !!!
[MCU2_0]     88.285186 s: UDMA: Init ... !!!
[MCU2_0]     88.286604 s: UDMA: Init ... Done !!!
[MCU2_0]     88.286681 s: MEM: Init ... !!!
[MCU2_0]     88.286726 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!!
[MCU2_0]     88.286800 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!!
[MCU2_0]     88.286864 s: MEM: Init ... Done !!!
[MCU2_0]     88.286892 s: IPC: Init ... !!!
[MCU2_0]     88.286961 s: IPC: 8 CPUs participating in IPC !!!
[MCU2_0]     88.287018 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_0]    100.306248 s: IPC: HLOS is ready !!!
[MCU2_0]    100.328017 s: IPC: Init ... Done !!!
[MCU2_0]    100.328098 s: APP: Syncing with 7 CPUs ... !!!
[MCU2_0]    101.171305 s: APP: Syncing with 7 CPUs ... Done !!!
[MCU2_0]    101.171538 s: REMOTE_SERVICE: Init ... !!!
[MCU2_0]    101.173464 s: [CAMERA_SUBSYSTEM]: Remote Service Init ...
[MCU2_0]    101.173540 s: [TIMESTAMP MODULE]: Remote Service Init ...
[MCU2_0]    101.173586 s: [TIMESTAMP MODULE]: Remote Service Init done.
[MCU2_0]    101.173624 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_0]    101.173670 s: ETHFW: Init FREERTOS ... !!!
[MCU2_0]    101.178662 s: Warning: Using 6 MAC address(es) from static pool
[MCU2_0]    101.178782 s: ETHFW: Shared multicasts (software fanout):
[MCU2_0]    101.178836 s:   01:00:5e:00:00:01
[MCU2_0]    101.178894 s: ETHFW: Reserved multicasts:
[MCU2_0]    101.178924 s:   01:80:c2:00:00:0e
[MCU2_0]    101.178977 s:   01:1b:19:00:00:00
[MCU2_0]    101.179415 s: EnetMcm: CPSW_9G on MAIN NAVSS
[MCU2_0]    101.192740 s: PHY 0 is alive
[MCU2_0]    101.193165 s: EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
[MCU2_0]    101.194919 s:
[MCU2_0] ETHFW Version   : 0.02.00
[MCU2_0]    101.194995 s: ETHFW Build Date: May 10, 2023
[MCU2_0]    101.195030 s: ETHFW Build Time: 14:33:12
[MCU2_0]    101.195058 s: ETHFW Commit SHA: 20f9a92c
[MCU2_0]    101.195133 s: ETHFW: Init ... DONE !!!
[MCU2_0]    101.195181 s: ETHFW: Remove server Init ... !!!
[MCU2_0]    101.195482 s: CpswProxyServer: Virtual port configuration:
[MCU2_0]    101.195557 s:   mpu_1_0 <-> Switch port 0: mpu_1_0_ethswitch-device-0
[MCU2_0]    101.196436 s: CpswProxyServer: initialization completed (core: mcu2_0)
[MCU2_0]    101.196507 s: ETHFW: Remove server Init ... DONE !!!
[MCU2_0]    101.197727 s: Starting lwIP, local interface IP is 192.168.1.200
[MCU2_0]    101.204464 s: Host MAC address: 70:ff:76:1d:92:c2
[MCU2_0]    101.208422 s: [LWIPIF_LWIP] Enet LLD netif initialized successfully
[MCU2_0]    101.238946 s: FVID2: Init ... !!!
[MCU2_0]    101.239059 s: FVID2: Init ... Done !!!
[MCU2_0]    101.239119 s: DSS: Init ... !!!
[MCU2_0]    101.239152 s: DSS: Display type is eDP !!!
[MCU2_0]    101.239184 s: DSS: M2M Path is enabled !!!
[MCU2_0]    101.239213 s: DSS: SoC init ... !!!
[MCU2_0]    101.239238 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2
[MCU2_0]    101.239478 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.239517 s: SCICLIENT: Sciclient_pmSetModuleState module=297 state=2
[MCU2_0]    101.239803 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.239856 s: SCICLIENT: Sciclient_pmSetModuleState module=151 state=2
[MCU2_0]    101.240037 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.240079 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11
[MCU2_0]    101.240210 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]    101.240247 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=13 parent=18
[MCU2_0]    101.240366 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]    101.240401 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=1 parent=2
[MCU2_0]    101.240556 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]    101.240610 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=1 freq=148500000
[MCU2_0]    101.241691 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success
[MCU2_0]    101.241747 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=1 state=2 flag=0
[MCU2_0]    101.241918 s: SCICLIENT: Sciclient_pmModuleClkRequest success
[MCU2_0]    101.241955 s: DSS: SoC init ... Done !!!
[MCU2_0]    101.241983 s: DSS: Board init ... !!!
[MCU2_0]    101.242089 s: DSS: Board init ... Done !!!
[MCU2_0]    101.259167 s: [LWIPIF_LWIP_IC] Interface started successfully
[MCU2_0]    101.259254 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[MCU2_0]    101.262186 s: DSS: Init ... Done !!!
[MCU2_0]    101.262254 s: VHWA: VPAC Init ... !!!
[MCU2_0]    101.262286 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2
[MCU2_0]    101.262513 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.262555 s: VHWA: LDC Init ... !!!
[MCU2_0]    101.266753 s: VHWA: LDC Init ... Done !!!
[MCU2_0]    101.266824 s: VHWA: MSC Init ... !!!
[MCU2_0]    101.280081 s: VHWA: MSC Init ... Done !!!
[MCU2_0]    101.280148 s: VHWA: NF Init ... !!!
[MCU2_0]    101.282239 s: VHWA: NF Init ... Done !!!
[MCU2_0]    101.282310 s: VHWA: VISS Init ... !!!
[MCU2_0]    101.294912 s: VHWA: VISS Init ... Done !!!
[MCU2_0]    101.294981 s: VHWA: VPAC Init ... Done !!!
[MCU2_0]    101.295156 s:  VX_ZONE_INIT:Enabled
[MCU2_0]    101.295190 s:  VX_ZONE_ERROR:Enabled
[MCU2_0]    101.295219 s:  VX_ZONE_WARNING:Enabled
[MCU2_0]    101.296764 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target MCU2-0
[MCU2_0]    101.297038 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target VPAC_NF
[MCU2_0]    101.297280 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target VPAC_LDC1
[MCU2_0]    101.297733 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target VPAC_MSC1
[MCU2_0]    101.297989 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target VPAC_MSC2
[MCU2_0]    101.298439 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target VPAC_VISS1
[MCU2_0]    101.298737 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE1
[MCU2_0]    101.299147 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE2
[MCU2_0]    101.299458 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DISPLAY1
[MCU2_0]    101.299889 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DISPLAY2
[MCU2_0]    101.300173 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CSITX
[MCU2_0]    101.300615 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE3
[MCU2_0]    101.300927 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE4
[MCU2_0]    101.301359 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE5
[MCU2_0]    101.301668 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE6
[MCU2_0]    101.302103 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE7
[MCU2_0]    101.302420 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target CAPTURE8
[MCU2_0]    101.302840 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DSS_M2M1
[MCU2_0]    101.303130 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DSS_M2M2
[MCU2_0]    101.303381 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DSS_M2M3
[MCU2_0]    101.303824 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DSS_M2M4
[MCU2_0]    101.303890 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU2_0]    101.303927 s: APP: OpenVX Target kernel init ... !!!
[MCU2_0]    101.328971 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetIpuKernels:102] IPU LOAD
[MCU2_0]    101.329208 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_0]    101.329257 s: CSI2RX: Init ... !!!
[MCU2_0]    101.329287 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]    101.329436 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.329480 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2
[MCU2_0]    101.329679 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.329738 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2
[MCU2_0]    101.329907 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.329942 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2
[MCU2_0]    101.330049 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.330084 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2
[MCU2_0]    101.330188 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.331079 s: CSI2RX: Init ... Done !!!
[MCU2_0]    101.331290 s: CSI2TX: Init ... !!!
[MCU2_0]    101.331321 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]    101.331458 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.331499 s: SCICLIENT: Sciclient_pmSetModuleState module=28 state=2
[MCU2_0]    101.331669 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.331703 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2
[MCU2_0]    101.331847 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]    101.332612 s: CSI2TX: Init ... Done !!!
[MCU2_0]    101.332814 s: ISS: Init ... !!!
[MCU2_0]    101.332868 s: NULL SENSOR init successfull.
[MCU2_0]    101.332903 s: IssSensor_Init ... Done !!!
[MCU2_0]    101.332998 s: IttRemoteServer_Init ... Done !!!
[MCU2_0]    101.333037 s: VISS REMOTE SERVICE: Init ... !!!
[MCU2_0]    101.333111 s: VISS REMOTE SERVICE: Init ... Done !!!
[MCU2_0]    101.333149 s: UDMA Copy: Init ... !!!
[MCU2_0]    101.335061 s: UDMA Copy: Init ... Done !!!
[MCU2_0]    101.338041 s: [CAMERA SUBSYSTEM] GPIO expander init DONE.
[MCU2_0]    101.338113 s: APP: Init ... Done !!!
[MCU2_0]    101.338147 s: APP: Run ... !!!
[MCU2_0]    101.338174 s: IPC: Starting echo test ...
[MCU2_0]    101.342695 s: APP: Run ... Done !!!
[MCU2_0]    101.370809 s: [LWIPIF_LWIP_IC] Interface started successfully
[MCU2_0]    101.370885 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[MCU2_0]    101.371003 s: Added interface 'br4', IP is 192.168.1.200
[MCU2_0]    101.373709 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] mcu3_0[.] mcu3_1[.] C66X_1[P] C66X_2[x] C7X_1[.]
[MCU2_0]    101.374295 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] mcu3_0[P] mcu3_1[.] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_0]    101.374439 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_0]    101.374636 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[.] C7X_1[P]
[MCU2_0]    101.374762 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[.] C7X_1[P]
[MCU2_0]    101.375026 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU2_0]    101.388452 s: EthFw: TimeSync PTP enabled
[MCU2_0]    101.393502 s: Rx Flow for Software Inter-VLAN Routing is up
[MCU2_0]    101.903383 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6
[MCU2_0]    104.811873 s: Cpsw_handleLinkUp: Port 6: Link up: 1-Gbps Full-Duplex
[MCU2_0]    105.609295 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c2, FlowIdx:172, FlowIdxOffset:0
[MCU2_0]    105.609605 s: Cpsw_ioctlInternal: CPSW: Registered MAC address. ALE entry:10, Policer Entry:3
[MCU2_0]    105.636881 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.643051 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:0:5e:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.648772 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:33:33:ff:1d:92:c2, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.670670 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:fb, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.705672 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:0, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.709337 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.712940 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:e, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.713099 s: CpswProxyServer_isRsvdMcast: Reserved mcast cannot be added to filter
[MCU2_0]    105.725572 s: Function:CpswProxyServer_registerIpv4MacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c2 IPv4Addr:192.168.1.20
[MCU2_0]    105.725796 s:
[MCU2_0]  SNo.      IP Address          MAC Address
[MCU2_0]    105.725843 s: ------    -------------     -----------------
[MCU2_0]    105.725884 s:   1       192.168.1.20     70:ff:76:1d:92:c2
[MCU2_0]    105.728408 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:0:5e:0:0:fb, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    105.736505 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:1:0:5e:0:0:fc, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    106.006537 s: CpswCpts_ioctl: Eth RX event not found (msgType=2, seqId=256, dom=0, portNum=5)
[MCU2_0]    107.004178 s: CpswCpts_ioctl: Eth RX event not found (msgType=2, seqId=256, dom=0, portNum=5)
[MCU2_0]    107.461249 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38b627c,CoreKey:38acb7e6, MacAddress:33:33:0:1:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0
[MCU2_0]    108.007767 s: CpswCpts_ioctl: Eth RX event not found (msgType=2, seqId=256, dom=0, portNum=5)
[MCU2_1]     88.232178 s: CIO: Init ... Done !!!
[MCU2_1]     88.232251 s: ### CPU Frequency = 1000000000 Hz
[MCU2_1]     88.232298 s: APP: Init ... !!!
[MCU2_1]     88.232327 s: SCICLIENT: Init ... !!!
[MCU2_1]     88.232599 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[MCU2_1]     88.232649 s: SCICLIENT: DMSC FW revision 0x8
[MCU2_1]     88.232689 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_1]     88.232730 s: SCICLIENT: Init ... Done !!!
[MCU2_1]     88.232758 s: UDMA: Init ... !!!
[MCU2_1]     88.234350 s: UDMA: Init ... Done !!!
[MCU2_1]     88.234412 s: MEM: Init ... !!!
[MCU2_1]     88.234460 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!!
[MCU2_1]     88.234545 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!!
[MCU2_1]     88.234610 s: MEM: Init ... Done !!!
[MCU2_1]     88.234640 s: IPC: Init ... !!!
[MCU2_1]     88.234707 s: IPC: 8 CPUs participating in IPC !!!
[MCU2_1]     88.234777 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_1]    100.624236 s: IPC: HLOS is ready !!!
[MCU2_1]    100.645899 s: IPC: Init ... Done !!!
[MCU2_1]    100.645972 s: APP: Syncing with 7 CPUs ... !!!
[MCU2_1]    101.171307 s: APP: Syncing with 7 CPUs ... Done !!!
[MCU2_1]    101.171534 s: REMOTE_SERVICE: Init ... !!!
[MCU2_1]    101.173501 s: [CAMERA_SUBSYSTEM]: Remote Service Init ...
[MCU2_1]    101.173578 s: [TIMESTAMP MODULE]: Remote Service Init ...
[MCU2_1]    101.173625 s: [TIMESTAMP MODULE]: Remote Service Init done.
[MCU2_1]    101.173662 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_1]    101.173698 s: FVID2: Init ... !!!
[MCU2_1]    101.173772 s: FVID2: Init ... Done !!!
[MCU2_1]    101.173807 s: VHWA: DMPAC: Init ... !!!
[MCU2_1]    101.173836 s: SCICLIENT: Sciclient_pmSetModuleState module=48 state=2
[MCU2_1]    101.174070 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]    101.174113 s: SCICLIENT: Sciclient_pmSetModuleState module=305 state=2
[MCU2_1]    101.174606 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]    101.174642 s: VHWA: DOF Init ... !!!
[MCU2_1]    101.184200 s: VHWA: DOF Init ... Done !!!
[MCU2_1]    101.184271 s: VHWA: SDE Init ... !!!
[MCU2_1]    101.186920 s: VHWA: SDE Init ... Done !!!
[MCU2_1]    101.186982 s: VHWA: DMPAC: Init ... Done !!!
[MCU2_1]    101.187030 s:  VX_ZONE_INIT:Enabled
[MCU2_1]    101.187067 s:  VX_ZONE_ERROR:Enabled
[MCU2_1]    101.187096 s:  VX_ZONE_WARNING:Enabled
[MCU2_1]    101.188304 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DMPAC_SDE
[MCU2_1]    101.188536 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target DMPAC_DOF
[MCU2_1]    101.188779 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target MCU2-1
[MCU2_1]    101.188840 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU2_1]    101.188879 s: APP: OpenVX Target kernel init ... !!!
[MCU2_1]    101.189184 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetIpuKernels:102] IPU LOAD
[MCU2_1]    101.189293 s:  VX_ZONE_ERROR:[tivxAddTargetKernelAdc:243] tivxAddTargetKernelByName
[MCU2_1]    101.189354 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_1]    101.189399 s: UDMA Copy: Init ... !!!
[MCU2_1]    101.191329 s: UDMA Copy: Init ... Done !!!
[MCU2_1]    101.191401 s: APP: Init ... Done !!!
[MCU2_1]    101.191436 s: APP: Run ... !!!
[MCU2_1]    101.191461 s: IPC: Starting echo test ...
[MCU2_1]    101.195013 s: APP: Run ... Done !!!
[MCU2_1]    101.196497 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] mcu3_0[.] mcu3_1[.] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_1]    101.197049 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] mcu3_0[P] mcu3_1[.] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_1]    101.197184 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_1]    101.197303 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[.]
[MCU2_1]    101.197487 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU2_1]    101.373336 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_0]     88.268299 s: CIO: Init ... Done !!!
[MCU3_0]     88.268378 s: ### CPU Frequency = 1000000000 Hz
[MCU3_0]     88.268424 s: APP: Init ... !!!
[MCU3_0]     88.268452 s: SCICLIENT: Init ... !!!
[MCU3_0]     88.268737 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[MCU3_0]     88.268798 s: SCICLIENT: DMSC FW revision 0x8
[MCU3_0]     88.268835 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU3_0]     88.268873 s: SCICLIENT: Init ... Done !!!
[MCU3_0]     88.268900 s: MEM: Init ... !!!
[MCU3_0]     88.268938 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ db000000 of size 8388608 bytes !!!
[MCU3_0]     88.269005 s: MEM: Init ... Done !!!
[MCU3_0]     88.269033 s: IPC: Init ... !!!
[MCU3_0]     88.269097 s: IPC: 8 CPUs participating in IPC !!!
[MCU3_0]     88.269150 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU3_0]    100.981897 s: IPC: HLOS is ready !!!
[MCU3_0]    101.003556 s: IPC: Init ... Done !!!
[MCU3_0]    101.003628 s: APP: Syncing with 7 CPUs ... !!!
[MCU3_0]    101.171305 s: APP: Syncing with 7 CPUs ... Done !!!
[MCU3_0]    101.171363 s: REMOTE_SERVICE: Init ... !!!
[MCU3_0]    101.173627 s: [CAMERA_SUBSYSTEM]: Remote Service Init ...
[MCU3_0]    101.173708 s: [TIMESTAMP MODULE]: Remote Service Init ...
[MCU3_0]    101.173748 s: [TIMESTAMP MODULE]: Remote Service Init done.
[MCU3_0]    101.173780 s: REMOTE_SERVICE: Init ... Done !!!
[MCU3_0]    101.173831 s:  VX_ZONE_INIT:Enabled
[MCU3_0]    101.173859 s:  VX_ZONE_ERROR:Enabled
[MCU3_0]    101.173887 s:  VX_ZONE_WARNING:Enabled
[MCU3_0]    101.175039 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target MCU3-0
[MCU3_0]    101.175108 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU3_0]    101.175148 s: APP: OpenVX Target kernel init ... !!!
[MCU3_0]    101.175188 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetIpuKernels:102] IPU LOAD
[MCU3_0]    101.175238 s: APP: OpenVX Target kernel init ... Done !!!
[MCU3_0]    101.175274 s: APP: Init ... Done !!!
[MCU3_0]    101.175302 s: APP: Run ... !!!
[MCU3_0]    101.175325 s: IPC: Starting echo test ...
[MCU3_0]    101.178942 s: APP: Run ... Done !!!
[MCU3_0]    101.180300 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[s] mcu3_1[.] C66X_1[x] C66X_2[x] C7X_1[P]
[MCU3_0]    101.181045 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[s] mcu3_1[P] C66X_1[.] C66X_2[.] C7X_1[P]
[MCU3_0]    101.181384 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[s] mcu3_1[P] C66X_1[.] C66X_2[P] C7X_1[P]
[MCU3_0]    101.181510 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[s] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_0]    101.197007 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] mcu3_0[s] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_0]    101.373358 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] mcu3_0[s] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_1]     88.305970 s: CIO: Init ... Done !!!
[MCU3_1]     88.306045 s: ### CPU Frequency = 1000000000 Hz
[MCU3_1]     88.306085 s: APP: Init ... !!!
[MCU3_1]     88.306110 s: SCICLIENT: Init ... !!!
[MCU3_1]     88.306393 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[MCU3_1]     88.306451 s: SCICLIENT: DMSC FW revision 0x8
[MCU3_1]     88.306485 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU3_1]     88.306521 s: SCICLIENT: Init ... Done !!!
[MCU3_1]     88.306548 s: MEM: Init ... !!!
[MCU3_1]     88.306587 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ db800000 of size 8388608 bytes !!!
[MCU3_1]     88.306655 s: MEM: Init ... Done !!!
[MCU3_1]     88.306682 s: IPC: Init ... !!!
[MCU3_1]     88.306747 s: IPC: 8 CPUs participating in IPC !!!
[MCU3_1]     88.306798 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU3_1]    101.150038 s: IPC: HLOS is ready !!!
[MCU3_1]    101.171183 s: IPC: Init ... Done !!!
[MCU3_1]    101.171255 s: APP: Syncing with 7 CPUs ... !!!
[MCU3_1]    101.171306 s: APP: Syncing with 7 CPUs ... Done !!!
[MCU3_1]    101.171343 s: REMOTE_SERVICE: Init ... !!!
[MCU3_1]    101.173624 s: [CAMERA_SUBSYSTEM]: Remote Service Init ...
[MCU3_1]    101.173705 s: [TIMESTAMP MODULE]: Remote Service Init ...
[MCU3_1]    101.173746 s: [TIMESTAMP MODULE]: Remote Service Init done.
[MCU3_1]    101.173780 s: REMOTE_SERVICE: Init ... Done !!!
[MCU3_1]    101.173833 s:  VX_ZONE_INIT:Enabled
[MCU3_1]    101.173862 s:  VX_ZONE_ERROR:Enabled
[MCU3_1]    101.173888 s:  VX_ZONE_WARNING:Enabled
[MCU3_1]    101.175041 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:64] Added target MCU3-1
[MCU3_1]    101.175103 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU3_1]    101.175141 s: APP: OpenVX Target kernel init ... !!!
[MCU3_1]    101.175180 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetIpuKernels:102] IPU LOAD
[MCU3_1]    101.175227 s: APP: OpenVX Target kernel init ... Done !!!
[MCU3_1]    101.175261 s: APP: Init ... Done !!!
[MCU3_1]    101.175288 s: APP: Run ... !!!
[MCU3_1]    101.175311 s: IPC: Starting echo test ...
[MCU3_1]    101.178924 s: APP: Run ... Done !!!
[MCU3_1]    101.180302 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[s] C66X_1[x] C66X_2[x] C7X_1[P]
[MCU3_1]    101.181029 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[s] C66X_1[.] C66X_2[.] C7X_1[P]
[MCU3_1]    101.181362 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[s] C66X_1[.] C66X_2[P] C7X_1[P]
[MCU3_1]    101.181495 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_1]    101.197030 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] mcu3_0[P] mcu3_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU3_1]    101.373389 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] mcu3_0[P] mcu3_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[C6x_1 ]     88.356246 s: CIO: Init ... Done !!!
[C6x_1 ]     88.356272 s: ### CPU Frequency = 1350000000 Hz
[C6x_1 ]     88.356282 s: APP: Init ... !!!
[C6x_1 ]     88.356290 s: SCICLIENT: Init ... !!!
[C6x_1 ]     88.356504 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[C6x_1 ]     88.356518 s: SCICLIENT: DMSC FW revision 0x8
[C6x_1 ]     88.356527 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_1 ]     88.356538 s: SCICLIENT: Init ... Done !!!
[C6x_1 ]     88.356547 s: UDMA: Init ... !!!
[C6x_1 ]     88.358090 s: UDMA: Init ... Done !!!
[C6x_1 ]     88.358111 s: MEM: Init ... !!!
[C6x_1 ]     88.358125 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ dc000000 of size 16777216 bytes !!!
[C6x_1 ]     88.358143 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_1 ]     88.358158 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ dd000000 of size 50331648 bytes !!!
[C6x_1 ]     88.358174 s: MEM: Init ... Done !!!
[C6x_1 ]     88.358183 s: IPC: Init ... !!!
[C6x_1 ]     88.358202 s: IPC: 8 CPUs participating in IPC !!!
[C6x_1 ]     88.358217 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_1 ]     99.557907 s: IPC: HLOS is ready !!!
[C6x_1 ]     99.562554 s: IPC: Init ... Done !!!
[C6x_1 ]     99.562582 s: APP: Syncing with 7 CPUs ... !!!
[C6x_1 ]    101.171305 s: APP: Syncing with 7 CPUs ... Done !!!
[C6x_1 ]    101.171319 s: REMOTE_SERVICE: Init ... !!!
[C6x_1 ]    101.172156 s: [TIMESTAMP MODULE]: Remote Service Init ...
[C6x_1 ]    101.172196 s: [TIMESTAMP MODULE]: Remote Service Init done.
[C6x_1 ]    101.172209 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_1 ]    101.172232 s:  VX_ZONE_INIT:Enabled
[C6x_1 ]    101.172242 s:  VX_ZONE_ERROR:Enabled
[C6x_1 ]    101.172252 s:  VX_ZONE_WARNING:Enabled
[C6x_1 ]    101.173189 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C6x_1 ]    101.173209 s: APP: OpenVX Target kernel init ... !!!
[C6x_1 ]    101.173840 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetC66Kernels:102] DSP LOAD
[C6x_1 ]    101.173861 s:  VX_ZONE_WARNING:[tivxAddTargetKernelCustomAdd:183] DSP tivxAddTargetKernelCustomAdd
[C6x_1 ]    101.173954 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_1 ]    101.173970 s: UDMA Copy: Init ... !!!
[C6x_1 ]    101.178544 s: UDMA Copy: Init ... Done !!!
[C6x_1 ]    101.178571 s: APP: Init ... Done !!!
[C6x_1 ]    101.178583 s: APP: Run ... !!!
[C6x_1 ]    101.178594 s: IPC: Starting echo test ...
[C6x_1 ]    101.180490 s: APP: Run ... Done !!!
[C6x_1 ]    101.180919 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[.] C66X_1[s] C66X_2[.] C7X_1[P]
[C6x_1 ]    101.181021 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[.] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]    101.181295 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]    101.181359 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]    101.196860 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]    101.373179 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_2 ]     88.448059 s: CIO: Init ... Done !!!
[C6x_2 ]     88.448087 s: ### CPU Frequency = 1350000000 Hz
[C6x_2 ]     88.448098 s: APP: Init ... !!!
[C6x_2 ]     88.448106 s: SCICLIENT: Init ... !!!
[C6x_2 ]     88.448345 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[C6x_2 ]     88.448359 s: SCICLIENT: DMSC FW revision 0x8
[C6x_2 ]     88.448369 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_2 ]     88.448380 s: SCICLIENT: Init ... Done !!!
[C6x_2 ]     88.448390 s: UDMA: Init ... !!!
[C6x_2 ]     88.449956 s: UDMA: Init ... Done !!!
[C6x_2 ]     88.449979 s: MEM: Init ... !!!
[C6x_2 ]     88.449993 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ e0000000 of size 16777216 bytes !!!
[C6x_2 ]     88.450011 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_2 ]     88.450027 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e1000000 of size 50331648 bytes !!!
[C6x_2 ]     88.450044 s: MEM: Init ... Done !!!
[C6x_2 ]     88.450053 s: IPC: Init ... !!!
[C6x_2 ]     88.450074 s: IPC: 8 CPUs participating in IPC !!!
[C6x_2 ]     88.450088 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_2 ]     99.879453 s: IPC: HLOS is ready !!!
[C6x_2 ]     99.883779 s: IPC: Init ... Done !!!
[C6x_2 ]     99.883808 s: APP: Syncing with 7 CPUs ... !!!
[C6x_2 ]    101.171306 s: APP: Syncing with 7 CPUs ... Done !!!
[C6x_2 ]    101.171319 s: REMOTE_SERVICE: Init ... !!!
[C6x_2 ]    101.172170 s: [TIMESTAMP MODULE]: Remote Service Init ...
[C6x_2 ]    101.172210 s: [TIMESTAMP MODULE]: Remote Service Init done.
[C6x_2 ]    101.172224 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_2 ]    101.172245 s:  VX_ZONE_INIT:Enabled
[C6x_2 ]    101.172256 s:  VX_ZONE_ERROR:Enabled
[C6x_2 ]    101.172269 s:  VX_ZONE_WARNING:Enabled
[C6x_2 ]    101.173198 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C6x_2 ]    101.173215 s: APP: OpenVX Target kernel init ... !!!
[C6x_2 ]    101.173865 s:  VX_ZONE_WARNING:[tivxRegisterCustomAddTargetC66Kernels:102] DSP LOAD
[C6x_2 ]    101.173887 s:  VX_ZONE_WARNING:[tivxAddTargetKernelCustomAdd:183] DSP tivxAddTargetKernelCustomAdd
[C6x_2 ]    101.173948 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_2 ]    101.173962 s: UDMA Copy: Init ... !!!
[C6x_2 ]    101.178172 s: UDMA Copy: Init ... Done !!!
[C6x_2 ]    101.178196 s: APP: Init ... Done !!!
[C6x_2 ]    101.178206 s: APP: Run ... !!!
[C6x_2 ]    101.178215 s: IPC: Starting echo test ...
[C6x_2 ]    101.180060 s: APP: Run ... Done !!!
[C6x_2 ]    101.180443 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[.] C66X_1[x] C66X_2[s] C7X_1[P]
[C6x_2 ]    101.180794 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[.] mcu3_1[P] C66X_1[.] C66X_2[s] C7X_1[P]
[C6x_2 ]    101.180842 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[.] C66X_2[s] C7X_1[P]
[C6x_2 ]    101.181002 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C6x_2 ]    101.196912 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C6x_2 ]    101.373228 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C7x_1 ]     89.008837 s: CIO: Init ... Done !!!
[C7x_1 ]     89.008850 s: ### CPU Frequency = 1000000000 Hz
[C7x_1 ]     89.008862 s: APP: Init ... !!!
[C7x_1 ]     89.008870 s: SCICLIENT: Init ... !!!
[C7x_1 ]     89.009108 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi]
[C7x_1 ]     89.009122 s: SCICLIENT: DMSC FW revision 0x8
[C7x_1 ]     89.009133 s: SCICLIENT: DMSC FW ABI revision 3.1
[C7x_1 ]     89.009144 s: SCICLIENT: Init ... Done !!!
[C7x_1 ]     89.009153 s: UDMA: Init ... !!!
[C7x_1 ]     89.010364 s: UDMA: Init ... Done !!!
[C7x_1 ]     89.010377 s: MEM: Init ... !!!
[C7x_1 ]     89.010388 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 117000000 of size 268435456 bytes !!!
[C7x_1 ]     89.010408 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!!
[C7x_1 ]     89.010426 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!!
[C7x_1 ]     89.010443 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!!
[C7x_1 ]     89.010461 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ 100000000 of size 385875968 bytes !!!
[C7x_1 ]     89.010479 s: MEM: Init ... Done !!!
[C7x_1 ]     89.010487 s: IPC: Init ... !!!
[C7x_1 ]     89.010501 s: IPC: 8 CPUs participating in IPC !!!
[C7x_1 ]     89.010515 s: IPC: Waiting for HLOS to be ready ... !!!
[C7x_1 ]    100.752455 s: IPC: HLOS is ready !!!
[C7x_1 ]    100.754903 s: IPC: Init ... Done !!!
[C7x_1 ]    100.754919 s: APP: Syncing with 7 CPUs ... !!!
[C7x_1 ]    101.171306 s: APP: Syncing with 7 CPUs ... Done !!!
[C7x_1 ]    101.171325 s: REMOTE_SERVICE: Init ... !!!
[C7x_1 ]    101.171510 s: REMOTE_SERVICE: Init ... Done !!!
[C7x_1 ]    101.171534 s:  VX_ZONE_INIT:Enabled
[C7x_1 ]    101.171546 s:  VX_ZONE_ERROR:Enabled
[C7x_1 ]    101.171556 s:  VX_ZONE_WARNING:Enabled
[C7x_1 ]    101.171731 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1
[C7x_1 ]    101.171807 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2
[C7x_1 ]    101.171916 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3
[C7x_1 ]    101.172052 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4
[C7x_1 ]    101.172170 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5
[C7x_1 ]    101.172247 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6
[C7x_1 ]    101.172379 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7
[C7x_1 ]    101.172476 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8
[C7x_1 ]    101.172502 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C7x_1 ]    101.172515 s: APP: OpenVX Target kernel init ... !!!
[C7x_1 ]    101.172707 s: APP: OpenVX Target kernel init ... Done !!!
APP: Init ... !!!
[C7x_1 ]    101.172721 s: APP: Init ... Done !!!
[C7x_1 ]    101.172731 s: APP: Run ... !!!
[C7x_1 ]    101.172741 s: IPC: Starting echo test ...
[C7x_1 ]    101.173007 s: APP: Run ... Done !!!
[C7x_1 ]    101.180092 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[.] C66X_1[x] C66X_2[x] C7X_1[s]
[C7x_1 ]    101.180137 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[x] C66X_2[x] C7X_1[s]
[C7x_1 ]    101.180444 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[x] C66X_2[P] C7X_1[s]
[C7x_1 ]    101.180889 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[s]
[C7x_1 ]    101.196938 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[s]
[C7x_1 ]    101.373261 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] mcu3_0[P] mcu3_1[P] C66X_1[P] C66X_2[P] C7X_1[s]

We analyzed this log, noticed the following lines:

[MCU2_0]    101.197727 s: Starting lwIP, local interface IP is 192.168.1.200

[MCU2_0] 101.370885 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[MCU2_0] 101.371003 s: Added interface 'br4', IP is 192.168.1.200

[MCU2_0]    104.811873 s: Cpsw_handleLinkUp: Port 6: Link up: 1-Gbps Full-Duplex

[MCU2_0] SNo. IP Address MAC Address
[MCU2_0] 105.725843 s: ------ ------------- -----------------
[MCU2_0] 105.725884 s: 1 192.168.1.20 70:ff:76:1d:92:c2

And then this:

[MCU2_0]    107.004178 s: CpswCpts_ioctl: Eth RX event not found (msgType=2, seqId=256, dom=0, portNum=5)

Are we missing any additional configuration or code changes that are requried for CPSW9g static IP configuration?

Best regards,

Ogi.