Other Parts Discussed in Thread: OMAPL138
hello,
My board type is omapl138,recently i read edma_test.c from ti(will give below) ,imitate its edma3_memtomemcpytest_dma_link function,write my own edma3 program.my purpose is trying to get audio signal,the result is i can get the signal forever but i can not do any operation about linux system like ping ifconfig ls etc.It seems the system is dead except receiving audio signal.My program is the same as test's edma3_memtomemcpytest_dma_link function,the only difference is the configuration of param_set,i think it is not the reason for this problem,maybe something wrong with the set of param_set.opt(the edma_test.c is OK),maybe need more for setting param_set.opt.Could you give me some suggestion on how to deal with this problem or how to find the problem.thanks!
my mcbsp_dma_rx_callback is like:
static void mcbsp_dma_rx_callback(unsigned lch, u16 ch_status, void *data)
{
int i = 0;
switch(ch_status) {
case DMA_COMPLETE:
printk ("From Callback 1: Channel %d status is: %u\n",lch, ch_status);
for(i = 0; i < BUFFSIZE; i++){
printk("%02x ",bufdest1[i]);
}
printk("\n");
for(i = 0; i < BUFFSIZE; i++){
printk("%02x ",bufdest2[i]);
}
printk("\n\n\n");
break;
case DMA_CC_ERROR:
printk ("\nFrom Callback 1: DMA_CC_ERROR occured "
"on Channel %d status is: %u\n", lch, ch_status);
break;
default:
printk ("\nFrom Callback 2: DMA_CC_ERROR occured "
"on Channel %d status is: %u\n", lch, ch_status);
break;
}
}
with this function i can make sure i have gotten the right signal.
and edma_test.c from ti is like:
/*
* file edma_test.c
* brief EDMA3 Test Application
*
* This file contains EDMA3 Test code.
*
* NOTE: THIS FILE IS PROVIDED ONLY FOR INITIAL DEMO RELEASE AND MAY BE
* REMOVED AFTER THE DEMO OR THE CONTENTS OF THIS FILE ARE SUBJECT
* TO CHANGE.
*
* @author Anuj Aggarwal
* @version 0.1 -
* Created on 30/09/05
* Assumption: Channel and ParamEntry has 1 to 1 mapping
* 0.2 - Sudhakar Rajashekhara
* 06/04/2009 - Modified to use new EDMA APIs
*/
#include <linux/module.h>
#include <linux/init.h>
#include <linux/errno.h>
#include <linux/types.h>
#include <linux/interrupt.h>
#include <asm/io.h>
#include <linux/moduleparam.h>
#include <linux/sysctl.h>
#include <linux/mm.h>
#include <linux/dma-mapping.h>
#include <mach/memory.h>
#include <mach/hardware.h>
#include <mach/irqs.h>
#include <mach/edma.h>
#undef EDMA3_DEBUG
/*#define EDMA3_DEBUG*/
#ifdef EDMA3_DEBUG
#define DMA_PRINTK(ARGS...) printk(KERN_INFO "<%s>: ",__FUNCTION__);printk(ARGS)
#define DMA_FN_IN printk(KERN_INFO "[%s]: start\n", __FUNCTION__)
#define DMA_FN_OUT printk(KERN_INFO "[%s]: end\n",__FUNCTION__)
#else
#define DMA_PRINTK( x... )
#define DMA_FN_IN
#define DMA_FN_OUT
#endif
#define MAX_DMA_TRANSFER_IN_BYTES (32768)
#define STATIC_SHIFT 3
#define TCINTEN_SHIFT 20
#define ITCINTEN_SHIFT 21
#define TCCHEN_SHIFT 22
#define ITCCHEN_SHIFT 23
static volatile int irqraised1 = 0;
static volatile int irqraised2 = 0;
int edma3_memtomemcpytest_dma(int acnt, int bcnt, int ccnt, int sync_mode, int event_queue);
int edma3_memtomemcpytest_dma_link(int acnt, int bcnt, int ccnt, int sync_mode, int event_queue);
int edma3_memtomemcpytest_dma_chain(int acnt, int bcnt, int ccnt, int sync_mode, int event_queue);
dma_addr_t dmaphyssrc1 = 0;
dma_addr_t dmaphyssrc2 = 0;
dma_addr_t dmaphysdest1 = 0;
dma_addr_t dmaphysdest2 = 0;
char *dmabufsrc1 = NULL;
char *dmabufsrc2 = NULL;
char *dmabufdest1 = NULL;
char *dmabufdest2 = NULL;
static int acnt = 512;
static int bcnt = 8;
static int ccnt = 8;
module_param(acnt, int, S_IRUGO);
module_param(bcnt, int, S_IRUGO);
module_param(ccnt, int, S_IRUGO);
static void callback1(unsigned lch, u16 ch_status, void *data)
{
//printk("******callback1******\n");
switch(ch_status) {
case DMA_COMPLETE:
irqraised1 = 1;
/*DMA_PRINTK ("\n From Callback 1: Channel %d status is: %u\n",
lch, ch_status);*/
break;
case DMA_CC_ERROR:
irqraised1 = -1;
DMA_PRINTK ("\nFrom Callback 1: DMA_CC_ERROR occured "
"on Channel %d\n", lch);
break;
default:
break;
}
}
static void callback2(unsigned lch, u16 ch_status, void *data)
{
switch(ch_status) {
case DMA_COMPLETE: //=1
irqraised2 = 1;
/*DMA_PRINTK ("\n From Callback 1: Channel %d status is: %u\n",
lch, ch_status);*/
break;
case DMA_CC_ERROR://=2
irqraised2 = -1;
DMA_PRINTK ("\nFrom Callback 1: DMA_CC_ERROR occured "
"on Channel %d\n", lch);
break;
default:
break;
}
}
static int __init edma_test_init(void)
{
int result = 0;
int iterations = 0;
int numTCs = 2;
int modes = 2;
int i,j;
printk ("\nInitializing edma_test module\n");
DMA_PRINTK ( "\nACNT=%d, BCNT=%d, CCNT=%d", acnt, bcnt, ccnt);
/* allocate consistent memory for DMA
* dmaphyssrc1(handle)= device viewed address.
* dmabufsrc1 = CPU-viewed address
*/
dmabufsrc1 = dma_alloc_coherent (NULL, MAX_DMA_TRANSFER_IN_BYTES,
&dmaphyssrc1, 0);
if (!dmabufsrc1) {
DMA_PRINTK ("dma_alloc_coherent failed for dmaphyssrc1\n");
return -ENOMEM;
}
dmabufdest1 = dma_alloc_coherent (NULL, MAX_DMA_TRANSFER_IN_BYTES,
&dmaphysdest1, 0);
if (!dmabufdest1) {
DMA_PRINTK("dma_alloc_coherent failed for dmaphysdest1\n");
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc1,
dmaphyssrc1);
return -ENOMEM;
}
dmabufsrc2 = dma_alloc_coherent (NULL, MAX_DMA_TRANSFER_IN_BYTES,
&dmaphyssrc2, 0);
if (!dmabufsrc2) {
DMA_PRINTK ("dma_alloc_coherent failed for dmaphyssrc2\n");
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc1,
dmaphyssrc1);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufdest1,
dmaphysdest1);
return -ENOMEM;
}
dmabufdest2 = dma_alloc_coherent (NULL, MAX_DMA_TRANSFER_IN_BYTES,
&dmaphysdest2, 0);
if (!dmabufdest2) {
DMA_PRINTK ("dma_alloc_coherent failed for dmaphysdest2\n");
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc1,
dmaphyssrc1);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufdest1,
dmaphysdest1);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc2,
dmaphyssrc2);
return -ENOMEM;
}
for (iterations = 0 ; iterations < 10 ; iterations++) {
DMA_PRINTK ("Iteration = %d\n", iterations);
for (j = 0 ; j < numTCs ; j++) { //TC
DMA_PRINTK ("TC = %d\n", j);
for (i = 0 ; i < modes ; i++) { //sync_mode
DMA_PRINTK ("Mode = %d\n", i);
/* Run all EDMA3 test cases */
DMA_PRINTK ("Starting edma3_memtomemcpytest_dma\n");
result = edma3_memtomemcpytest_dma(acnt, bcnt, ccnt, i, j);
if (0 == result) {
printk("edma3_memtomemcpytest_dma passed\n");
} else {
printk("edma3_memtomemcpytest_dma failed\n");
}
if (0 == result) {
DMA_PRINTK ("Starting edma3_memtomemcpytest_dma_link\n");
result = edma3_memtomemcpytest_dma_link(acnt, bcnt, ccnt, i, j);
if (0 == result) {
printk("edma3_memtomemcpytest_dma_link passed\n");
} else {
printk("edma3_memtomemcpytest_dma_link failed\n");
}
}
if (0 == result) {
DMA_PRINTK ("Starting edma3_memtomemcpytest_dma_chain\n");
result = edma3_memtomemcpytest_dma_chain(acnt, bcnt, ccnt, i, j);
if (0 == result) {
printk("edma3_memtomemcpytest_dma_chain passed\n");
} else {
printk("edma3_memtomemcpytest_dma_chain failed\n");
}
}
}
}
}
return result;
}
void edma_test_exit(void)
{
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc1, dmaphyssrc1);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufdest1,
dmaphysdest1);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufsrc2, dmaphyssrc2);
dma_free_coherent(NULL, MAX_DMA_TRANSFER_IN_BYTES, dmabufdest2,
dmaphysdest2);
printk ("\nExiting edma_test module\n");
}
/* DMA Channel, Mem-2-Mem Copy, ASYNC Mode, INCR Mode */
int edma3_memtomemcpytest_dma (int acnt, int bcnt, int ccnt, int sync_mode, int event_queue)
{
int result = 0;
unsigned int dma_ch = 0;
int i;
int count = 0;
unsigned int Istestpassed = 0u;
unsigned int numenabled = 0;
unsigned int BRCnt = 0;
int srcbidx = 0;
int desbidx = 0;
int srccidx = 0;
int descidx = 0;
struct edmacc_param param_set;
/* Initalize source and destination buffers */
for (count = 0u; count < (acnt*bcnt*ccnt); count++) {
dmabufsrc1[count] = 'A' + (count % 26);
dmabufdest1[count] = 0;
}
/* Set B count reload as B count. */
BRCnt = bcnt;
/* Setting up the SRC/DES Index */
srcbidx = acnt;
desbidx = acnt;
/* A Sync Transfer Mode */
srccidx = acnt;
descidx = acnt;
result = edma_alloc_channel (EDMA_CHANNEL_ANY, callback1, NULL, event_queue);
if (result < 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma::edma_alloc_channel failed for dma_ch, error:%d\n", result);
return result;
}
dma_ch = result;
edma_set_src (dma_ch, (unsigned long)(dmaphyssrc1), INCR, W8BIT);
edma_set_dest (dma_ch, (unsigned long)(dmaphysdest1), INCR, W8BIT);
edma_set_src_index (dma_ch, srcbidx, srccidx);
edma_set_dest_index (dma_ch, desbidx, descidx);
/* A Sync Transfer Mode */
edma_set_transfer_params (dma_ch, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 1 */
edma_read_slot (dma_ch, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch));
edma_write_slot (dma_ch, ¶m_set);
numenabled = bcnt * ccnt;
for (i = 0; i < numenabled; i++) {
irqraised1 = 0;
/*
* Now enable the transfer as many times as calculated above.
*/
result = edma_start(dma_ch);
if (result != 0) {
DMA_PRINTK ("edma3_memtomemcpytest_dma: davinci_start_dma failed \n");
break;
}
/* Wait for the Completion ISR. */
while (irqraised1 == 0u);
/* Check the status of the completed transfer */
if (irqraised1 < 0) {
/* Some error occured, break from the FOR loop. */
DMA_PRINTK ("edma3_memtomemcpytest_dma: Event Miss Occured!!!\n");
break;
}
}
if (0 == result) {
for (i = 0; i < (acnt*bcnt*ccnt); i++) {
if (dmabufsrc1[i] != dmabufdest1[i]) {
DMA_PRINTK ("\n edma3_memtomemcpytest_dma: Data write-read matching failed at = %u\n",i);
Istestpassed = 0u;
break;
}
}
if (i == (acnt*bcnt*ccnt))
Istestpassed = 1u;
edma_stop(dma_ch);
edma_free_channel(dma_ch);
}
if (Istestpassed == 1u) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma: EDMA Data Transfer Successfull \n");
} else {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma: EDMA Data Transfer Failed \n");
}
return result;
}
/* 2 DMA Channels Linked, Mem-2-Mem Copy, ASYNC Mode, INCR Mode */
int edma3_memtomemcpytest_dma_link(int acnt, int bcnt, int ccnt, int sync_mode, int event_queue)
{
int result = 0;
unsigned int dma_ch1 = 0;
unsigned int dma_ch2 = 0;
int i;
int count = 0;
unsigned int Istestpassed1 = 0u;
unsigned int Istestpassed2 = 0u;
unsigned int numenabled = 0;
unsigned int BRCnt = 0;
int srcbidx = 0;
int desbidx = 0;
int srccidx = 0;
int descidx = 0;
struct edmacc_param param_set;
/* Initalize source and destination buffers */
for (count = 0u; count < (acnt*bcnt*ccnt); count++) {
dmabufsrc1[count] = 'A' + (count % 26);
dmabufdest1[count] = 0;
dmabufsrc2[count] = 'A' + (count % 26);
dmabufdest2[count] = 0;
}
/* Set B count reload as B count. */
BRCnt = bcnt;
/* Setting up the SRC/DES Index */
srcbidx = acnt;
desbidx = acnt;
/* A Sync Transfer Mode */
srccidx = acnt;
descidx = acnt;
result = edma_alloc_channel (EDMA_CHANNEL_ANY, callback1, NULL, event_queue);
if (result < 0) {
DMA_PRINTK ("edma3_memtomemcpytest_dma_link::edma_alloc_channel "
"failed for dma_ch1, error:%d\n", result);
return result;
}
dma_ch1 = result;
edma_set_src (dma_ch1, (unsigned long)(dmaphyssrc1), INCR, W8BIT);
edma_set_dest (dma_ch1, (unsigned long)(dmaphysdest1), INCR, W8BIT);
edma_set_src_index (dma_ch1, srcbidx, srccidx);
edma_set_dest_index (dma_ch1, desbidx, descidx);
edma_set_transfer_params (dma_ch1, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 1 */
edma_read_slot (dma_ch1, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch1));
edma_write_slot(dma_ch1, ¶m_set);
/* Request a Link Channel */
result = edma_alloc_slot (0, EDMA_SLOT_ANY);
if (result < 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link::edma_alloc_slot "
"failed for dma_ch2, error:%d\n", result);
return result;
}
dma_ch2 = result;
edma_set_src (dma_ch2, (unsigned long)(dmaphyssrc2), INCR, W8BIT);
edma_set_dest (dma_ch2, (unsigned long)(dmaphysdest2), INCR, W8BIT);
edma_set_src_index (dma_ch2, srcbidx, srccidx);
edma_set_dest_index (dma_ch2, desbidx, descidx);
edma_set_transfer_params (dma_ch2, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 2 */
edma_read_slot (dma_ch2, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch1));
edma_write_slot(dma_ch2, ¶m_set);
/* Link both the channels */
edma_link(dma_ch1, dma_ch2);
numenabled = bcnt * ccnt;
for (i = 0; i < numenabled; i++) {
irqraised1 = 0;
/*
* Now enable the transfer as many times as calculated above.
*/
result = edma_start(dma_ch1);
if (result != 0) {
DMA_PRINTK ("edma3_memtomemcpytest_dma_link: davinci_start_dma failed \n");
break;
}
/* Wait for the Completion ISR. */
//while (irqraised1 == 0u);//orig
while (irqraised1 == 0u)
{
//printk("********irqraised1 -> while-ing********\n");
}
/* Check the status of the completed transfer */
if (irqraised1 < 0) {
/* Some error occured, break from the FOR loop. */
DMA_PRINTK ("edma3_memtomemcpytest_dma_link: "
"Event Miss Occured!!!\n");
break;
}
}
if (result == 0) {
for (i = 0; i < numenabled; i++) {
irqraised1 = 0;
/*
* Now enable the transfer as many times as calculated above
* on the LINK channel.
*/
result = edma_start(dma_ch1);
if (result != 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link: davinci_start_dma failed \n");
break;
}
/* Wait for the Completion ISR. */
while (irqraised1 == 0u);
/* Check the status of the completed transfer */
if (irqraised1 < 0) {
/* Some error occured, break from the FOR loop. */
DMA_PRINTK ("edma3_memtomemcpytest_dma_link: "
"Event Miss Occured!!!\n");
break;
}
}
}
if (0 == result) {
for (i = 0; i < (acnt*bcnt*ccnt); i++) {
if (dmabufsrc1[i] != dmabufdest1[i]) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link(1): Data "
"write-read matching failed at = %u\n",i);
Istestpassed1 = 0u;
break;
}
}
if (i == (acnt*bcnt*ccnt)) {
Istestpassed1 = 1u;
}
for (i = 0; i < (acnt*bcnt*ccnt); i++) {
if (dmabufsrc2[i] != dmabufdest2[i]) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link(2): Data "
"write-read matching failed at = %u\n",i);
Istestpassed2 = 0u;
break;
}
}
if (i == (acnt*bcnt*ccnt)) {
Istestpassed2 = 1u;
}
edma_stop(dma_ch1);
edma_free_channel(dma_ch1);
edma_stop(dma_ch2);
edma_free_slot(dma_ch2);
edma_free_channel(dma_ch2);
}
if ((Istestpassed1 == 1u) && (Istestpassed2 == 1u)) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link: EDMA Data Transfer Successfull\n");
} else {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_link: EDMA Data Transfer Failed\n");
}
return result;
}
/* 2 DMA Channels Chained, Mem-2-Mem Copy, A-SYNC Mode, INCR Mode */
int edma3_memtomemcpytest_dma_chain(int acnt, int bcnt, int ccnt, int sync_mode, int event_queue)
{
int result = 0;
unsigned int dma_ch1 = 0;
unsigned int dma_ch2 = 0;
int i;
int count = 0;
unsigned int Istestpassed1 = 0u;
unsigned int Istestpassed2 = 0u;
unsigned int numenabled = 0;
unsigned int BRCnt = 0;
int srcbidx = 0;
int desbidx = 0;
int srccidx = 0;
int descidx = 0;
struct edmacc_param param_set;
/* Initalize source and destination buffers */
for (count = 0u; count < (acnt*bcnt*ccnt); count++) {
dmabufsrc1[count] = 'A' + (count % 26);
dmabufdest1[count] = 0;
dmabufsrc2[count] = 'A' + (count % 26);
dmabufdest2[count] = 0;
}
/* Set B count reload as B count. */
BRCnt = bcnt;
/* Setting up the SRC/DES Index */
srcbidx = acnt;
desbidx = acnt;
/* A Sync Transfer Mode */
srccidx = acnt;
descidx = acnt;
result = edma_alloc_channel (EDMA_CHANNEL_ANY, callback1, NULL, event_queue);
if (result < 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_chain::davinci_request_dma"
" failed for dma_ch1, error:%d\n", result);
return result;
}
dma_ch1 = result;
edma_set_src (dma_ch1, (unsigned long)(dmaphyssrc1), INCR, W8BIT);
edma_set_dest (dma_ch1, (unsigned long)(dmaphysdest1), INCR, W8BIT);
edma_set_src_index (dma_ch1, srcbidx, srccidx);
edma_set_dest_index (dma_ch1, desbidx, descidx);
edma_set_transfer_params (dma_ch1, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Request another DMA Channel */
result = edma_alloc_channel (EDMA_CHANNEL_ANY, callback2, NULL, event_queue);
if (result < 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_chain::davinci_request_dma "
"failed for dma_ch2, error:%d\n", result);
edma_free_channel(dma_ch1);
return result;
}
dma_ch2 = result;
edma_set_src (dma_ch2, (unsigned long)(dmaphyssrc2), INCR, W8BIT);
edma_set_dest (dma_ch2, (unsigned long)(dmaphysdest2), INCR, W8BIT);
edma_set_src_index (dma_ch2, srcbidx, srccidx);
edma_set_dest_index (dma_ch2, desbidx, descidx);
edma_set_transfer_params (dma_ch2, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Chain both the channels */
edma_read_slot(dma_ch1, ¶m_set);
param_set.opt |= (1 << TCCHEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch2));
edma_write_slot(dma_ch1, ¶m_set);
/*
* Enable the Intermediate and Final Interrupts on Channel 1.
* Also, Enable the Intermediate Chaining.
*/
edma_read_slot(dma_ch1, ¶m_set);
param_set.opt |= (1 << ITCCHEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= (1 << ITCINTEN_SHIFT);
edma_write_slot(dma_ch1, ¶m_set);
/* Enable the Intermediate and Final Interrupts on Channel 2 */
edma_read_slot(dma_ch2, ¶m_set);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= (1 << ITCINTEN_SHIFT);
edma_write_slot(dma_ch2, ¶m_set);
numenabled = bcnt * ccnt;
for (i = 0; i < numenabled; i++) {
irqraised2 = 0;
/*
* Now enable the transfer for Master channel as many times
* as calculated above.
*/
result = edma_start(dma_ch1);
if (result != 0) {
DMA_PRINTK ("\nedma3_memtomemcpytest_dma_chain: "
"davinci_start_dma failed \n");
edma_stop(dma_ch1);
edma_free_channel(dma_ch1);
edma_free_channel(dma_ch2);
return result;
}
/*
* Transfer on the master channel (ch1Id) will finish after some
* time.
* Now, because of the enabling of intermediate chaining on channel
* 1, after the transfer gets over, a sync event will be sent
* to channel 2, which will trigger the transfer on it.
* Also, Final and Intermediate Transfer Complete
* Interrupts are enabled on channel 2, so we should wait for the
* completion ISR on channel 2 first, before proceeding
* ahead.
*/
while (irqraised2 == 0u);
/* Check the status of the completed transfer */
if (irqraised2 < 0) {
/* Some error occured, break from the FOR loop. */
DMA_PRINTK ("edma3_test_with_chaining: "
"Event Miss Occured!!!\n");
break;
}
}
/* Match the Source and Destination Buffers. */
for (i = 0; i < (acnt*bcnt*ccnt); i++) {
if (dmabufsrc1[i] != dmabufdest1[i]) {
DMA_PRINTK ( "\nedma3_memtomemcpytest_dma_chain(1): Data write-read matching failed at = %u\n",i);
Istestpassed1 = 0u;
break;
}
}
if (i == (acnt*bcnt*ccnt)) {
Istestpassed1 = 1u;
}
for (i = 0; i < (acnt*bcnt*ccnt); i++) {
if (dmabufsrc2[i] != dmabufdest2[i]) {
DMA_PRINTK ( "\nedma3_memtomemcpytest_dma_chain(2): Data write-read matching failed at = %u\n",i);
Istestpassed2 = 0u;
break;
}
}
if (i == (acnt*bcnt*ccnt)) {
Istestpassed2 = 1u;
}
edma_stop(dma_ch1);
edma_free_channel(dma_ch1);
edma_stop(dma_ch2);
edma_free_slot(dma_ch2);
edma_free_channel(dma_ch2);
if((Istestpassed1 == 1u) && (Istestpassed2 == 1u)) {
DMA_PRINTK ( "\nedma3_memtomemcpytest_dma_chain: EDMA Data Transfer Successfull\n");
} else {
DMA_PRINTK ( "\nedma3_memtomemcpytest_dma_chain: EDMA Data Transfer Failed\n");
}
return result;
}
module_init(edma_test_init);
module_exit(edma_test_exit);
MODULE_AUTHOR("Texas Instruments");
MODULE_LICENSE("GPL");