Part Number: AM3354
Hi,
Good Day.
Which option do I have to increase the time between CS going low and the first SCLK? tlead in the picture (please see below)
We need 5 µs.

Please advise. Thank you very much.
Best Regards,
Ray Vincent
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3354
Hi,
Good Day.
Which option do I have to increase the time between CS going low and the first SCLK? tlead in the picture (please see below)
We need 5 µs.

Please advise. Thank you very much.
Best Regards,
Ray Vincent
Hello Vincent,
Thank you.
The below diagram provide the information.
Figure 24-6. Phase and Polarity Combinations
Looks like the delay is clock dependent.
Could you ask customer to elaborate the requirements and the need for the delay.
Based on the above diagram, I guess the delay is fixed based on the clock speed.
Regards,
Sreenivasa
Hi Sreenivasa,
Good Day.
We would like to request data from a sensor. To get actually data, the sensor uses the time between CS to SCLK to update its SPI output buffer with the latest sensor value.
Is it possible to switch the CS Pin manually (By HAL write function)? Or can I configure the CS Pin as GPIO (Output Pin) and not select this pin as CS Pin in SPI Interface? (maybe select one other pin which is not connected?)
Best Regards,
Ray Vincent
Hello Ray Vincent
Thank you for the inputs.
Is it possible to switch the CS Pin manually (By HAL write function)? Or can I configure the CS Pin as GPIO (Output Pin) and not select this pin as CS Pin in SPI Interface? (maybe select one other pin which is not connected?)
This could be a possible option. Do you have a setup to test?
Other option is to reduce the interface speed. Any thoughts on the speed requirement?
Regards,
Sreenivasa
Hi Sreenivasa,
Good Day.
Which could be a possible option?
Option 1:
Is it possible to switch the CS Pin manually (By HAL write function)?
Option 2:
Or can I configure the CS Pin as GPIO (Output Pin) and not select this pin as CS Pin in SPI Interface? (maybe select one other pin which is not connected?)
Which Option would you prefer?
Reducing interface Clock frequency is not really an option. We have to send 40 Bytes each 200µs. Currently, we have 3MHz and take about 140 -150 µs.
Best Regards,
Ray Vincent
Hello Ray Vincent
Good morning and thank you for the inputs.
Option 2:
Or can I configure the CS Pin as GPIO (Output Pin) and not select this pin as CS Pin in SPI Interface? (maybe select one other pin which is not connected?)
Which Option would you prefer?
I would assume this option provides implementation flexibility.
Option 1:
Is it possible to switch the CS Pin manually (By HAL write function)?
I will have to check on this method internally based on your requirement.
Regards,
Sreenivasa
Hi Sreenivasa,
Good Day. I would like to follow up on the customer's query. Thank you very much.
Best Regards,
Ray Vincent
Hello Ray Vincent
Thank you.
Please refer the answer i copied from the previous thread.
Good morning and thank you for the inputs.
Option 2:
Or can I configure the CS Pin as GPIO (Output Pin) and not select this pin as CS Pin in SPI Interface? (maybe select one other pin which is not connected?)
Which Option would you prefer?
Hello Ray Vincent
Pls refer below inputs i received from the device expert:
Normally, you could use TCS to increase the delay between CS and the first clock.
However, in this case, with a 3MHz clock, the maximum delay would only be 3.5 * 333ns = 1.16us. This is short of the required 5us.
The two alternate options, slowing the bit rate or manually controlling the CS are both valid.
Since, reducing the frequency is not an option, then it will be necessary to manually Controlling CS. It is documented in the TRM:
24.3.2.6 Single-Channel Master Mode
Manual control can be implemented by a GPO, but I believe the MCSPI_CHxCONF:FORCE bit can also be used. See TRM section reference above and see table 24-18.
There are restrictions which are documented in the TRM.
Regards,
Sreenivasa
Hello Ray Vincent
Just added your query regarding the findability in the TRM.
Please refer Page 4899 and page 4937.
Regards,
Sreenivasa