This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSPC6713B EMIF addressing problem?



I am developing a DSPC6713B board with an ALTER CPLD. The EMIF address is very strange.

When I used the CE2n space, the corresponding address for the following VHDL code is 0xA0080000:

assign CSAD1n = ~((~CE2n)& XA20 & (~XA19)& (~XA18));

When the CE3n is used, the corresponding address for the following VHDL code is 0xB0040000:

assign user_LED1 = ~((~CE3n)& XA20 & (~XA19) & (~XA18) & XD1);

It is just very confused for me! What is the  addressing method for EMIF address line EA2~EA21.

Is the EA2 corresponding the lowest address bit A0 or not?