Before run our application ,we are trying to load the module automatically through init.d (run the loadmodule.sh).The loadmodule script is executing,but we are getting in the attachement
========== Sample Application : helloDSP ========== Entered helloDSP_Create () dsplink driver open: /dev/dsplink: No such file or directory PROC_setup () failed. Status = [0x80008008] Leaving helloDSP_Create () Entered helloDSP_Delete () Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 478 MSGQ_release () failed. Status = [0x8000800b] Assertion failed (((drvObj != NULL) && (IS_OBJECT_VALID (drvObj, SIGN_DRV))) || ((drvObj == NULL) && (cmdId == CMD_PROC_ATTA1 Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 329 Leaving helloDSP_Delete () ==================================================== Segmentation fault