Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Hello sir,
TDA4VH: what's function will be used Low Freq Clock (32.768KHz)? If we don't use this mode, how to deal with WKUP_LP_CLKIN this pin?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I see in TDA4VH EVM, use an RTC provide frequency to this pin as input signal. My question is this frequency will be used to which internal module of TDA4VH?
BTW, if PMIC TPS6594133A external OSC 32K crystal in its side, we can use TPS6594133A GPIO to provide this frequency to TDA4VH By WKUP_LP_CLKIN pin, so that can reduce a RTC component?
Typically the CLKIN will be an option to clock timers.
WKUP_LP_CLKIN is an LVCMOS pin, so it should be OK to clock from an external component, including the PMIC if the voltage levels are compatible.
Kevin
If we don't want to use this pin, just left it is ok? Thus will have any impact for internal module features?
Cynthia
I hate leaving an LVCMOS pin floating. Pull the pin down either with an external resistor or with the internal pull-down available within the PADCONFIG registers.
You are not required to clock this signal; just don't use it for a timer...
Kevin