Hi,
I have never taken the role of the system engineer, so please do not assume I know anything about what I am trying to do.
Now that I have my audio program running on the DSP, with the help from CCS for loading the program. So I guess if I want to show it to someone without having to connect to a PC with CCS, I should
- find a flash burn program and use it to burn the .out file onto the flash.
- expect next time when it power up, it will boot from the flash and run the program.
So I am asking
- Where do I find this flash burn program?
- Is there an tutorial for this?
Thanks