Other Parts Discussed in Thread: TMDSEMU110-U, TM4C1294NCPDT
Hi team,
I am Using CCS along with TI XDS110 (TMDSEMU110-U)Debugger.
when i try to connect through the CCS,I am getting error as in the attachment.
Please Let me know your feedback
This utility has selected a 100/110/510 class product. This utility will load the adapter 'jioxds110.dll'. The library build date was 'Nov 28 2022'. The library build time was '16:30:46'. The library package version is '9.10.0.00080'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-260' (0xfffffefc). The title is 'SC_ERR_XDS110_OPEN'. The explanation is: An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. [End: Texas Instruments XDS110 USB Debug Probe_0]