This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: build linux kernel using bitbake

Part Number: PROCESSOR-SDK-AM62X

Hello,

I performed build by using Yocto project with bitbake.
At first I believed that linux kernel will be built by performing following command, however, it seemed that output include prebuild kernel image.

$ MACHINE=am62xx-evm  bitbake tisdk-base-image

Q1, Is my above understanding correct ?
Q2, If so, how I can build linux kernel ?
(Now, one of appling build linux kernel to linux system is using "make linux" under "ti-processor-sdk-linux-am62xx-evm-08.05.00.21/" folder by using following command.

$ make linux

and perform following command after completing build to  SD card which is implemented "tisdk-base-image".

$ sudo DESTDIR=/media/users/rootfs make linux_install

However, I would like to know how linux kernel should be built by using bitbake instead of make command.

BR,