This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash boot question for C6713

Hi,

I am using a C6713 DSP and have a couple of questions regarding Flash boot.

1) The bootmode pins are HD4, HD3 which have IPD, IPU respectively. So does this mean by default the

bootmode is set to EMIF Boot or Flash boot and we do not need to add any external PUs and PDs?

2) I was reading some post on e2e.ti (http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/86746/299580.aspx)

and read that HD13 also should have a 10k pull-up for it to function corectly. Is this still valid and do we need a pull-up on HD13?

3) I am trying to convert the .out file to .hex file using hex6x.exe. My question is do we have to initialize the PLL and EMIF registers

while using hex6x.exe? Is there an example .cmd file/ command line arguments that shows how to do it?

What are the other things that I need to look at while converting out file to hex file?

Thanks,

Aditi.