This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ftp performance issues over WiFi



 

Hi All,

We are using the TI Sitara AM37X Evaluation Module (EVM) Sitara (Win CE 6.0 R3)from Mistral for developing a handheld device

 TI WL1271 module is interfaced to the hardware for WiFi functionality.The performance tests for testing the file transfer functionality for a file download from laptop to EVM shows pathetic performance  .

The throughput is approximately 1-2Mbps .However iperf shows good throughput(18Mbps). Please let me know if anyone has observed this behavior.

The results repeats if tested on a wired network (eth interface of EVM) .Also the same ftp application and test setup works with good throughput on a competitor platform(EVM replaced)

 

Thanks,

Jithendran

 (Device/Laptop connected to AP,FTP server running on laptop)
Client application - Customer supplied Kerberos ftp application
Server application - Customer supplied Warftpd

------------------------------------------------------------------------------------------------------------