Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM
Hello sir,
I notice there is a VPEF module in TDA4VM, what's the function for this module?
BTW, for this module, has been removed from next product?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
VPFE is used to capture RAW data over parallel interface. But it is not supported in the SDK.
Yes, this module is only available on TDA4VM.
Regards,
Brijesh
For TDA4VM, VPFE this feature support in SDK?
What's the use case for VPFE module, is the same use case CSI-RX interface, can connect SerDes sensor using this?
Hi xin,
No SDK does not support this feature and as of now, no plan to support this module.
It is primarily used for capturing raw image frames over parallel interface.
Well from usage point of view, it is same case as CSIRX, but CSITX is serializer LVDS interface, whereas VPFE is digital parallel interface. SERDES can be used with VPFE if SERDES can output over parallel interface.
Regards,
Brijesh