Fisrt, something wrong occured when startup---messy code and undev failed as image below.
I used pre-images in AM35x-OMAP35x-PSP-SDK-03.00.01.06.tgz---include x-load.bin.ift、u-boot.bin、uImage、rootfs.jffs2 in file images, and Language of Tera Term is English.I don't know why.

2.matrix-gui-e does not exist in /etc/init.d/ even after I built Matrx GUI successully
When I make and install the Matrix GUI successfully as http://e2e.ti.com/support/embedded/f/354/t/121847.aspx, the next step is Matrix GUI Startup Debug as http://processors.wiki.ti.com/index.php/Matrix_Users_Guide#Matrix_GUI_Startup_Debug. However I found that matrix-gui-e did not exist in EVM(through the console of Tera Term), but exist in /home/user/ti-sdk-am3517-evm-05.02.00.00.targetNFS/etc/init.d/ in the host Ubuntu10.04. So I had to copy the related files(such as libgthread-2.0.0.so.0) to the EVM. However, when I use the command matrix-guiE, it reminded me that qt is not here-----as mentioned Launching Matrix of http://processors.wiki.ti.com/index.php/Matrix_Users_Guide#Matrix_GUI_Startup_Debug.
The “-qws” parameter is required to start the Qt window server if this is the only/first Qt application running on the system.
The “-display transformed:Rot90” parameter causes the Qt windowing system to rotate the display 90 degrees.
The question is HOW COULD I INSTLL QT and IS QI IS ESSENTIAL FOR MATRIX GUI? NO wiki. I found two related website:
http://doc.qt.nokia.com/4.6/qt-embedded-install.html and http://processors.wiki.ti.com/index.php/DM365_touchscreen_with_Qt
But I don't know if it's right.
Thank you!