Hi,
This is related with the followings thread.
I built the following source and got binary.
source C:\ti\sdk_am5716\processor_sdk_rtos_am57xx_08_01_00_09\pdk_am57xx_1_0_19\packages\ti\drv\pm\examples\cpuidle\main_a15.c
binary C:\ti\sdk_am5716\processor_sdk_rtos_am57xx_08_01_00_09\pdk_am57xx_1_0_19\packages\ti\binary\pm_cpuidle_testapp\bin\idkAM571x\pm_cpuidle_testapp_a15_0_release.xa15fg
Question 1
In original linker file, pcode and data is placed in DRAM. When I created binary using this linker and tried to loard binary on AM57x on CCS, it failed. Maybe DDR is not initialized.
So I changed the linker file to place code and data SRAM. I attached this linker file. Would you check if there are any issue?
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/lnk_5F00_a15.cmd
Question 2
I connected XDS110 to AM57 EVM.
<hardware>
This is the EVM I'm using.
.
<CCS>
I loaded binary to AM57 and ran A15 core. I captured my desktop and attached it below.
As this video shows
1) When I loaded binary, program counter did not stop at the beginning of main(). After I clicked CPU stop and restart icon, CPU stopped at the beginnig of main(). Is this method OK? Is their any propriate way to load binary ?
2) After 1), CPU started from main() and entered function "Board_watchdogDisable()" , CPU cannot exit from this function and cannot got to the next. Would advise how to fix it to go to the next ?
Thank you.
Best Regards,
Kasai