Hi all,
I understand that DM355 sdk has support for mt9t131 image
sensor but the leopardboard which
i am using has omnivision OM7725
sensor so i want to install drivers related to ov7725 sensor in the
kernel so that i can run
the examples/demo on the current board set up.Please guide me how can i
proceed doing that.
How can i make ov7725 work on my LeopardBoard.
i have seen some directory for mt9v113 patch:
DM355SDK789311/fs/fs/lib/
modules/2.6.29-ridgerun-davinci1/build/.pc/mt9v113-vga-sensor-support.patch/drivers/media/video/davinci
so do i have to do something similar to that in order to create drivers for ov7725.
Is it possible to run demos/examples and see the image captured by the camera on my board in the current set up.
Thanks and Regards,
Mayank
so do i have to do something similar to that in order to create drivers for ov7725.
Is it possible to run demos/examples and see the image captured by the camera on my board in the current set up.
Thanks and Regards,
Mayank